This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我根據"Sensorless Field Oriented Control of 3-Phase Induction Motors"
並測試完level 1後,點選 reset CPU
卻出現下列錯誤
====================================
Trouble Reading PC Register:
(Error -1142 @ 0x0)
Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.
(Emulation package 5.1.73.0)
====================================
出現此ERROR視窗後我點選強制啟動
並在點選RESET CPU一次
卻出現
下列錯誤
===================================
no source available for 0x3FF599
===================================
請問我該如何解決此問題??
有的,我暫停運轉後才執行RESET CPU。
另外有一個問題想請教
在LEVEL2~6中每個測試中叫出的4 個圖的物理值都不同
那在"GRAPH properties"裡的"Start AddressA"與"Start AddressB"的設定是否需要做相對的改變
還是一樣依照手冊裡的設定在"DLOG_4CH_buff1~4"?