For some reason, I need to run the float algorithm to generate the lib on one pc and then run the CLA routine on another computer with the lib.
I tried to use CLA feature, but the following warning appeared at build:
#10461-D Invalid to cal C28 function "Float calcula" defined in "DyT/C2000/foat lib2.ib<float calculaobi>' from CLA file "/asin.obj"(Here I use the lib library approach).
I have blocked all integer calculations and integer judgments in lib, and still report errors.
Is it because other forum posts discuss that.cla files cannot refer to functions in other.c files, only those algorithmic functions can be written in.cla files?