This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 是否可以配置EPWMxA占空比波形,xB配置带死区的高低电平

Part Number: TMS320F280049C

目前我们在做电机类的相关底层配置。是否能配置如下所示的波形?

我目前大概了解了一下,也许不全面,希望得到TI比较好的方法。目前我们使用hrpwm4,hrpwm5,hrpwm6。谢谢!

如图所示,图一位示例,图二为示波器实测波形,2B和3B因探头没有多余通道就没有测。

  • 从第一张示例来看是通过ePWM模块的PC斩波得到的。

    目前的方案是什么?

  • (1)目前我们的方案是有感BLDC电动工具,但是没有找到类似280049的有感BLDC电机驱动的工程。如果采用无感BLDC的280049工程再从2803x的有感BLDC移植过来这样可行?

    (2)我已从《HVBLDC_Sensored》的2803x的设计文件<f2803xbldcpwm.h>看到类似这样的配置,移植过来用示波器测试还没有发出波形。只有A是高电平,B是低电平,不配成互补波形的话,需要配哪些寄存器?这个地方对我来说还是比较难,能否有280049有感bldc六步换相跑得起来的寄存器配置?

    (3)我要做BLDC有感电动工具,建立比较好的工程,您有什么建议的?

    (4)以下是移植过来的配置寄存器代码

    EPwm4Regs.TBCTL.bit.SYNCOSEL = 0;
    EPwm5Regs.TBCTL.bit.SYNCOSEL = 0;
    EPwm6Regs.TBCTL.bit.SYNCOSEL = 0;

    /* Allow each timer to be sync'ed*/

    EPwm4Regs.TBCTL.bit.PHSEN = 1;
    EPwm5Regs.TBCTL.bit.PHSEN = 1;
    EPwm6Regs.TBCTL.bit.PHSEN = 1;

    /* Init Timer-Base Period Register for EPWM4-EPWM6*/
    EPwm4Regs.TBPRD = period;//v.PeriodMax;
    EPwm5Regs.TBPRD = period;//v.PeriodMax;
    EPwm6Regs.TBPRD = period;//v.PeriodMax;

    /* Init Timer-Base Phase Register for EPWM4-EPWM6*/
    EPwm4Regs.TBPHS.bit.TBPHS=0;//half.TBPHS = 0;
    EPwm5Regs.TBPHS.bit.TBPHS=0;//half.TBPHS = 0;
    EPwm6Regs.TBPHS.bit.TBPHS=0;//half.TBPHS = 0;

    /* Init Timer-Base Control Register for EPWM4-EPWM6*/
    EPwm4Regs.TBCTL.all = BLDCPWM_INIT_STATE;
    EPwm5Regs.TBCTL.all = BLDCPWM_INIT_STATE;
    EPwm6Regs.TBCTL.all = BLDCPWM_INIT_STATE;

    /* Init Compare Control Register for EPWM4-EPWM6 */
    EPwm4Regs.CMPCTL.all = BLDCPWM_CMPCTL_INIT_STATE;
    EPwm5Regs.CMPCTL.all = BLDCPWM_CMPCTL_INIT_STATE;
    EPwm6Regs.CMPCTL.all = BLDCPWM_CMPCTL_INIT_STATE;

    /* Init Action Qualifier Output A Register for EPWM4-EPWM6*/
    EPwm4Regs.AQCTLA.all = BLDCPWM_AQCTLA_INIT_STATE;
    EPwm5Regs.AQCTLA.all = BLDCPWM_AQCTLA_INIT_STATE;
    EPwm6Regs.AQCTLA.all = BLDCPWM_AQCTLA_INIT_STATE;

    /* Init Dead-Band Generator Control Register for EPWM4-EPWM6*/
    EPwm4Regs.DBCTL.all = BLDCPWM_DBCTL_INIT_STATE;
    EPwm5Regs.DBCTL.all = BLDCPWM_DBCTL_INIT_STATE;
    EPwm6Regs.DBCTL.all = BLDCPWM_DBCTL_INIT_STATE;

    /* Init PWM Chopper Control Register for EPWM4-EPWM6*/
    EPwm4Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;
    EPwm5Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;
    EPwm6Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;

    EALLOW; /* Enable EALLOW */


    /* Setting six EPWM as primary output pins*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; /* EPWM4A pin*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; /* EPWM4B pin*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; /* EPWM5A pin*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; /* EPWM5B pin*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; /* EPWM6A pin*/
    GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; /* EPWM6B pin*/

    EDIS; /* Disable EALLOW*/

    这是A+B-,其他换相类似。

    (*ePWM[ch4]).AQCSFRC.bit.CSFA = 0; /* Forcing disabledd on output A of EPWM4 */\
    (*ePWM[ch4]).AQCTLA.bit.CAU = 2; /* Set high when CTR = CMPA on UP-count */\
    (*ePWM[ch4]).AQCTLA.bit.ZRO = 1; /* Set low when CTR = Zero */\
    (*ePWM[ch4]).CMPA.half.CMPA = (int16)(Tmp>>15); /* PWM signal on output A of EPWM4 (Q15 -> Q0) */\
    (*ePWM[ch4).AQCSFRC.bit.CSFB = 1; /* Forcing a continuous Low on output B of EPWM4 */\
    /* */\
    (*ePWM[ch5]).AQCSFRC.bit.CSFA = 1; /* Forcing a continuous Low on output A of EPWM5 */\
    (*ePWM[ch5]).AQCSFRC.bit.CSFB = 2; /* Forcing a continuous High on output B of EPWM5 */\
    /* */\
    (*ePWM[ch6]).AQCSFRC.bit.CSFA = 1; /* Forcing a continuous Low on output A of EPWM6 */\
    (*ePWM[ch6]).AQCSFRC.bit.CSFB = 1; /* Forcing a continuous Low on output B of EPWM6

  • 1. 可以;

    2. 

    不配成互补波形的话,需要配哪些寄存器

    这个实现的方法有很多,简单来说配置比较点(COMP)并配合相应的动作(AQ)即可;

    能否有280049有感bldc六步换相跑得起来的寄存器配置?

    C2000实现的BLDC基本都是FOC;

    3. 如果是用六步换相做电动工具,有更低成本的MSPM0G系列可以选择,还有集成了控制器的BLDC驱动器;

    4. 

    /* Init PWM Chopper Control Register for EPWM4-EPWM6*/
    EPwm4Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;
    EPwm5Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;
    EPwm6Regs.PCCTL.all = BLDCPWM_PCCTL_INIT_STATE;

    结合代码来看,目前的波形应该是通过PC斩波得到的。

  • (1)上管是PWM,下管普通GPIO,我配出波形,电机转动有刺耳声。

    (2)MSPM0G这个方案TI有官方软硬件demo吗