Other Parts Discussed in Thread: TIDA-010062
我用flash烧写程序,每次下电后都需要再重新烧写一遍,GPIO24和GPIO32都上拉过了,用的例程是TIDA-010062,请问是还需要怎么配置一下吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用flash烧写程序,每次下电后都需要再重新烧写一遍,GPIO24和GPIO32都上拉过了,用的例程是TIDA-010062,请问是还需要怎么配置一下吗

是用的flash选项,boot模式选择是指的GPIO24和32都是高电平吗,我两个pin都是用的3.3V上拉
https://www.ti.com/lit/ug/tiduet7g/tiduet7g.pdf
请看一下第50页的3.1.5.4 Loading the Custom Bootloader and Application to Flash Using CCS
我直接import project的 ttplpfc f28003x文件中并没有Bank0_LDFU and Bank1_LDFU,我应该怎么把它添加到我的project里面呢,直接加入的话编译会报错。
在import的flash_kernel_ex3_sci_flash_kernel project中是可以选择的,是要先用这个程序去对mcu进行配置吗