Part Number: TMS320F28379D
估算器好像无法正常工作,请问一下要怎么解决哪?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考下工程师的回复:
Was customer running with their own motor? Can they confirm their motor parameters are accurate?
There is another finding that you mentioned in a previous thread that you have to change the "obj->oneOverDcBus_invV" from the estimator output to ADC feedback in level 2 for the motor to operate, but level 2 always uses the actual ADC data as shown below.

To debug the estimator, it would be better to make sure the estimator functions well in level 2 when the motor is running in open loop control.