Part Number: TMS320F280025
Dear team,
我在使用cmd文件遇到下面的问题:
.C文件里定义了一个段

1.放在指定地址
分配给指定地址,但是.map文件里找不到user1。

2.放在分配好的空间,.map文件里有分配出来的段,但是user1没有被放进去,也找不到.user1



(在之前的主程序里user1是分配成功过的,但是bootloader工程里分配失败)
请问是什么原因呢
Thanks,
Enya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025
Dear team,
我在使用cmd文件遇到下面的问题:
.C文件里定义了一个段

1.放在指定地址
分配给指定地址,但是.map文件里找不到user1。

2.放在分配好的空间,.map文件里有分配出来的段,但是user1没有被放进去,也找不到.user1



(在之前的主程序里user1是分配成功过的,但是bootloader工程里分配失败)
请问是什么原因呢
Thanks,
Enya
#pragma DATA_SECTION我也试过,还是不行,甚至尝试把数组改成结构体也是不行。目前区别只有指定的memory不同
图片是两个段的比较


下面是cmd文件里段指定的地址/memory。
MEMORY
{
BEGIN : origin = 0x00080000, length = 0x00000002
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMLS4 : origin = 0x0000A000, length = 0x00000800
RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAMLS6 : origin = 0x0000B000, length = 0x00000800
RAMLS7 : origin = 0x0000B800, length = 0x00000800*/
/* Combining all the LS RAMs */
RAMLS4567 : origin = 0x0000A000, length = 0x00002000
RAMGS0 : origin = 0x0000C000, length = 0x000007F0//
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
// FLASHBANK1 : origin = 0x00080000, length = 0x0000FFF0
// FLASH_BANK1_RSVD : origin = 0x0008FFF0, length = 0x00000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x001FF0 /* on-chip Flash0x000FFE */
USER1 : origin = 0x00081FF2, length = 0x00000004
// FLASH_BANK0_SEC1 : origin = 0x080100, length = 0x001F00 /* on-chip Flash */
BEGIN_MAIN : origin = 0x082000, length = 0x000002
FLASH_BANK0_SEC2 : origin = 0x082002, length = 0x004FFE /* on-chip Flash */
// FLASH_BANK0_SEC3 : origin = 0x082100, length = 0x001900 /* on-chip Flash */
// FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
// FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
// FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0 /* on-chip Flash */
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
//#define MAIN
#define BOOT
SECTIONS
{
#ifdef BOOT
codestart : > BEGIN, ALIGN(8)
.text : > FLASH_BANK0_SEC0, ALIGN(8)
.cinit : > FLASH_BANK0_SEC0, ALIGN(8)
.switch : > FLASH_BANK0_SEC0, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
.init_array : > FLASH_BANK0_SEC0, ALIGN(8)
.bss : > RAMLS4567
.bss:output : > RAMLS4567
.bss:cio : > RAMGS0
.const : > FLASH_BANK0_SEC0, ALIGN(8)
.data : > RAMLS4567
.sysmem : > RAMLS4567
.user1 : > USER1
.sec_noinit : > 0x0000C7E0, TYPE = NOINIT, PAGE = 1
#else
codestart : > BEGIN_MAIN, ALIGN(8)
.text : >> FLASH_BANK0_SEC2, ALIGN(8)
.cinit : > FLASH_BANK0_SEC2, ALIGN(8)
.switch : > FLASH_BANK0_SEC2, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
.init_array : > FLASH_BANK0_SEC2, ALIGN(8)
.bss : > RAMLS4567
.bss:output : > RAMLS4567
.bss:cio : > RAMGS0
.const : > FLASH_BANK0_SEC2, ALIGN(8)
.data : > RAMLS4567
.sysmem : > RAMLS4567
.user2 : > 0x082208, PAGE = 1
.sec_noinit : > 0x0000C7E0, TYPE = NOINIT, PAGE = 1
#endif
ramgs0 : > RAMGS0
/* Allocate IQ math areas: */
IQmath : > RAMLS4567
IQmathTables : > RAMLS4567
.TI.ramfunc : LOAD = FLASH_BANK0_SEC0,
RUN = RAMGS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
DataBufferSection : > RAMLS4567, ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/