以下是我连接和烧录dsp28335遇到的问题,也已经尝试了重新安装CCS3.3和XDS560的驱动,还是不起作用。
连接另外的机器正常。
我的上电顺序:1.电脑连接仿真器 2.连接JTAG口 3.打开CCS3.3 4.DSP28335上电 5.通过CCS平台连接DSP
Win7系统,仿真器SEED-XDS560PLUS ,编程环境:CCS3.3.38.2
1.仿真器连接不上28335(BGA封装)
错误信息提示如下:
打卡CCS:
Error connecting to the target: Error 0x80000240/-233 Fatal Error during: I
nitialization, OCS, This error was generated by TI's USCIF driver.
SC_ERR_PTH_BROKEN <-233> An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken with a stuck-at-ones or stuck-at-zero fault.
再次点connect:
Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
Error connecting to the target: Error 0x80000200/-1037 Fatal Error during: OCS, PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
2.以前遇到过仿真器不能够烧录flash,却能够在RAM里运行程序,这个肯定是flash锁死的问题
对于第一个问题,很是莫名其妙,基本的连接都没有连接上。