This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: 程序可下载但不运行且无法仿真;

Part Number: TMS320F28075


现象:

1、使用芯片为TMS320F28075PZPT,通过JTAG下载器进行下载进Flash,程序可正常下载成功,断电启动后程序不能正常运行,GPIO72与GPIO84引导接口为高电平,XRS_N引脚稳定为高电平,VDD引脚电平已经为1.2V,晶振高低电平满足芯片要求,频率为20.000MHz;

2、通过软件下载到ARM进入调试模式后,界面如下所示;通过软件复位与硬件复位不能改变这种情况;

3、此现象在百张板卡中,存在两张此类板卡情况;

问题1:请问以上情况可能是由什么原因导致的?可以大概确定是硬件上还是软件上的问题吗?

问题2:有什么方法可以检测并处理到以上的问题吗?