Part Number: TMS320F28075
现象:
1、使用芯片为TMS320F28075PZPT,通过JTAG下载器进行下载进Flash,程序可正常下载成功,断电启动后程序不能正常运行,GPIO72与GPIO84引导接口为高电平,XRS_N引脚稳定为高电平,VDD引脚电平已经为1.2V,晶振高低电平满足芯片要求,频率为20.000MHz;
2、通过软件下载到ARM进入调试模式后,界面如下所示;通过软件复位与硬件复位不能改变这种情况;
3、此现象在百张板卡中,存在两张此类板卡情况;
问题1:请问以上情况可能是由什么原因导致的?可以大概确定是硬件上还是软件上的问题吗?
问题2:有什么方法可以检测并处理到以上的问题吗?