This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我看到手册中有这样一张图,那么CAN和DSP本身可以采用不同的晶振吗?
可以的
你好,我用CAN_selectClockSource(CANA_BASE,CAN_CLOCK_SOURCE_XTAL);这一函数定义了CAN的晶振,但我发现定义了以后CAN模块没有输出并且也无法读,外部晶振是20MHz,内部是10MHz,请问是还有其他地方需要设置吗?
不能用外部晶振,是外部时钟,之前回复的不是很准确。