This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: ECAP检测

Part Number: TMS320F28335


在引脚上通过信号源输入ECAP检测的方波,发现ECAP检测到的值是方波的毛刺所在的地方,而不是程序设置的方波下降沿。如果方波波形没有毛刺的话,ECAP就会检测不到数据。具体的配置如下:

    ECap4Regs.ECCTL1.bit.CAP1POL = 1;// 0;       //0 => Rising Edge; 1 => Falling Edge;
    ECap4Regs.ECCTL1.bit.CTRRST1 = 0;       //0 => Do not reset counter
    ECap4Regs.ECCTL1.bit.CAPLDEN = 1;       //1 => Enable cap load
    ECap4Regs.ECCTL1.bit.PRESCALE = 0;      //0 => Bypass the prescaler

    ECap4Regs.ECCTL2.bit.CAP_APWM = 0;      //0 => Capture mode; 1 => APWM mode
    ECap4Regs.ECCTL2.bit.CONT_ONESHT = 1;   //1 => One shoot mode
    ECap4Regs.ECCTL2.bit.SYNCO_SEL = 3;     //3 => Disable synchronous signal out
    ECap4Regs.ECCTL2.bit.SYNCI_EN = 1;      //1 => Enable synchronous
    ECap4Regs.ECCTL2.bit.STOP_WRAP = 0;     //n => Stop capture sequence after event n + 1
    ECap4Regs.ECCTL2.bit.TSCTRSTOP = 1;     //1 => Allow TSCTR to run

    ECap4Regs.CTRPHS = 0;                   //Synchronous Phase

    ECap4Regs.ECEINT.bit.CEVT1 = 0;         //1 => Enable interrupt for event 1