如果是可以用作GPIO,为什么我没看到配置GPO的输出值的寄存器呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为这款器件EtherCAT的PDI接口没有数字I/O功能,所以为这款器件的EtherCAT增加了GPI以及GPO。

spruiz1a_TMS320F28P65x Real-Time Microcontrollers Technical Reference Manual (Rev. A)第4493页26.1.6.3 General-Purpose Inputs and Outputs
具体的配置请产看第4510页26.2.9 General-Purpose Inputs and Outputs
我看下列寄存器都是配置GPI/O的寄存器,配置完成后如何去使用呢?比如我某个引脚想输出一个高电平,因为我没找到相关的寄存器

这个GPI/GPO功能是给EtherCAT使用的。如果想给MCU用,直接用GPIO就好。
Hi Yale,
我就是想给ESC用,但是我没理解手册中的意思,这个GPI/GPO是如何使用起来的呢?