Other Parts Discussed in Thread: TLV3502
使用TLV3502输出了一个方波波形作为ECAP的检测信号,ECAP3和ECAP4的管脚分别设置为GPIO9和GPIO11,发现方波信号在不与GPIO连接前输出正确,连接后电平出现偏差,想请问一下是否是配置的问题?
下面波形中红色的是方波信号,前一张是接入前,后一张是接入后。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用TLV3502输出了一个方波波形作为ECAP的检测信号,ECAP3和ECAP4的管脚分别设置为GPIO9和GPIO11,发现方波信号在不与GPIO连接前输出正确,连接后电平出现偏差,想请问一下是否是配置的问题?
下面波形中红色的是方波信号,前一张是接入前,后一张是接入后。


GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 3; //ECAP3
GpioCtrlRegs.GPAPUD.bit.GPIO9=1; //禁止上拉使能
GpioCtrlRegs.GPADIR.bit.GPIO9=0; //配置成输入
GpioCtrlRegs.GPAQSEL1.bit.GPIO9 = 2; // 0=>Sync to SysClock; 1=>3*Tsa; 2=>6*Ts
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 3; //ECAP4
GpioCtrlRegs.GPAPUD.bit.GPIO11=1; //禁止上拉使能
GpioCtrlRegs.GPADIR.bit.GPIO11=0; //配置成输入
GpioCtrlRegs.GPAQSEL1.bit.GPIO11 = 2; // 0=>Sync to SysClock; 1=>3*Tsa; 2=>6*Ts
配置成这样也不能正常工作,波形和图上的一致