首先,请问TMS320F28335 的ADC需要做准确的3.0V超压保护电路吗?
从数据手册的原理框图里,没有看到自带的保护电路呢
我们项目中模拟量输入可能偶尔会出现超压,为了不牺牲精度,所以不愿再做缩放。
Hardware Design Guidelines for TMS320F28xx and TMS320F28xxx DSCs 文中这样写道:
It is necessary to maintain the analog input voltage applied to the ADCIN pins within
0 V – 3.0 V range. These analog signals pass through the multiplexer network first. Any
voltage above VDDA + 0.3 V or below VSS – 0.3 V will bias the multiplexer in an undesired way,
giving the wrong values for other channels. To achieve accurate values, the sample
capacitor should be charged to within ½ LSB of the final value.
TMS320F28xx/28xxx DSCs 模拟接口设计综述 文中这样写道:
用在模拟转换器输入引脚上的电压应该严格限制在0 V–3 V,如果在任何通道上,超过了这个范围,就会
暂时影响到其他通道的转换。如果用于输入模拟信号的数字电路需要使用任何高的电压(5V)供电, 在
连接到模数转换器的输入引脚之前,推荐采用缓冲状态缩放信号使之小于3 V。
其次是超压保护电路的实现:
《手把手学DSP》上提供的二极管钳位电路,实际限制电压为电源电压+二极管导通电压,有 3.3+0.7 = 4V,比3.0V高了不少。
如果需要准确的3.0V超压保护,电路如何实现也是个问题。
请问大家有没有在设计中有遇到和解决这样关于28335 ADC 的问题呀?
谢谢