在一个逆变电源产品上运行良好的程序(当时开发的工程项目第一版是在2018年,当时安装的CCS版本为5.5版,后来在2021年又改了一版程序。现在换用64位WIN11系统,安装过CCS不同版本,例如,8.3.1,9.3.0,10.2.0,11.0.0,12.7.0,加载2021年第2版这个工程项目,部分CCS能显示源代码,但就是不能编译BUILD.如果编译,会显示如下错误提示。从提示中,本人分析需要安装C2000V20.12 compiler,但通过官网没发现有对应的CCS版本),
Import failed for project 'LCP2S' because its compiler definition is not available. Please install the C2000 v20.12 compiler before importing this project:
- See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update.
- Visit CCS App Center to get the latest compiler support.
- Or download and install the compiler [http://software-dl.ti.com/codegen/non-esd/downloads], then register it with CCS through 'Preferences > CCS > Build > Compilers