Part Number: TMS320F28335
新手小白问一个问题,在数据表上看到F28335“数据读取总线和数据写入总线各由 32 条地址线和 32 条数据线组成”,但片上存储空间一共4M,22根数据地址就够了,为什么这里数据的地址线要强调32条呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
新手小白问一个问题,在数据表上看到F28335“数据读取总线和数据写入总线各由 32 条地址线和 32 条数据线组成”,但片上存储空间一共4M,22根数据地址就够了,为什么这里数据的地址线要强调32条呢?
您好
TMS320F28335是一款32位浮点DSP处理器,其数据地址总线设计为32根有特定的原因,尽管其片上存储空间可能并不需要全部的32位地址线来寻址。以下是对这一设计的解释:
32位处理器架构:TMS320F28335是一款32位处理器,这意味着它的内部寄存器和主要的数据处理单元都是基于32位宽度的。为了与这种架构相匹配,地址和数据总线也需要是32位,以便在一次操作中能够完整地传输32位的数据或地址。
哈佛结构:该DSP采用哈佛结构,这种结构将程序存储器和数据存储器分开,允许同时访问指令和数据,从而提高了处理速度。在这种结构中,32位地址总线可以独立地用于程序存储器和数据存储器的寻址,使得处理器能够高效地同时处理指令和数据。
外部扩展性:虽然TMS320F28335的片上存储空间可能只需要22根地址线来完全寻址,但强调32条地址线可能还考虑到了外部存储扩展的需要。通过更多的地址线,处理器可以寻址更大的外部存储空间,这为系统提供了更大的灵活性和可扩展性。
兼容性和标准化:在设计处理器时,为了保持与TI公司其他32位DSP产品的兼容性和实现设计的标准化,也会选择使用32位地址和数据总线。这种设计选择有助于简化硬件和软件的开发流程。
综上所述,尽管TMS320F28335的片上存储空间可能不需要全部的32位地址线来寻址,但出于处理器架构、哈佛结构、外部扩展性以及兼容性和标准化的考虑,设计师仍然选择了32条地址线的设计。这样的设计使得该DSP在处理复杂任务时能够更加高效和灵活。