This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ePWM相位调整问题?



在调整相位的过程中有点问题,

EPwm1Regs.CMPA.half.CMPA = 835; 
EPwm1Regs.CMPB = 745; 
EPwm1Regs.TBPRD = 1580;

EPwm2Regs.CMPA.half.CMPA = 835; 
EPwm2Regs.CMPB = 745; 
EPwm2Regs.TBPRD = 1580;

EPwm2Regs.TBPHS.half.TBPHS = 0;

现象是:

1.逐步增加相位差(即EPwm2Regs.TBPHS.half.TBPHS逐渐增大,每次加1,最大不超过周期EPwm1Regs.TBPRD = 1580),一切正常。

2.但是,再向下减相位时(即EPwm2Regs.TBPHS.half.TBPHS逐渐减少,每次减1,减到0为止),在两个点有问题,EPwm2Regs.TBPHS.half.TBPHS = 835时(刚好是CMPA 的值),再向下减1(即EPwm2Regs.TBPHS.half.TBPHS = 834,有嗒的一声),在EPwm2Regs.TBPHS.half.TBPHS = 745时(刚好是CMPB 值),再向下减1(即EPwm2Regs.TBPHS.half.TBPHS = 744,有嗒的一声),请问这是什么原因,应该不是巧合,是不是那个地方配置还有问题,求解?

初始化代码如下:

void InitEPwm1(void)
{

// Enable TZ1 and TZ2 as one shot trip sources
EALLOW;
EPwm1Regs.TZSEL.bit.OSHT1 = 1;
EPwm1Regs.TZSEL.bit.OSHT2 = 1;

// What do we want the TZ1 and TZ2 to do?
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_HI;
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_HI;

// Enable TZ interrupt
//EPwm1Regs.TZEINT.bit.OST = 1;
EDIS;


// Setup TBCLK
EPwm1Regs.TBPRD =EPWM1_TIMER_TBPRD; //600; // Set timer period 801 TBCLKs
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
//EPwm1Regs.TBCTL.bit.PRDLD = 0;

// Set Compare values
EPwm1Regs.CMPA.half.CMPA = EPWM1_MIN_CMPA;//324;//; // Set compare A value
EPwm1Regs.CMPB = EPWM1_MIN_CMPB;//276;//; // Set Compare B value

// Setup counter mode
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
//EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;//0x0-1分频,TBCLK = SYSCLKOUT / (HSPCLKDIV × CLKDIV)

EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module

// Setup shadowing
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

#if 1
// Action Qualifier SubModule Registers
//EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;//AQ_CLEAR;
//EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;//AQ_SET;

EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;//AQ_CLEAR;
EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;//AQ_SET;
EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm1Regs.AQCTLB.bit.CBD = AQ_CLEAR;
#endif


#if 1
// Interrupt where we will change the Compare Values
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTRU_CMPB;//ET_CTR_ZERO; // Select INT on Zero event
mPWM1_Disable(); // Disable INT ,close pwm disable,open pwm enable
EPwm1Regs.ETPS.bit.INTPRD = ET_2ND; // Generate INT on 3rd event
#endif

#if 1

EALLOW;
//===========================================================================
// TZA events can force EPWMxA
// TZB events can force EPWMxB
#if 1
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_HI; // EPWM1A will go low //故障产生时的保护
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_HI; // EPWM1B will go low
#endif
EPwm1Regs.TZFRC.bit.OST = 1; // Turn off the PWM

EDIS;
#endif

}


void InitEPwm2(void)
{
#if 1
// Enable TZ1 and TZ2 as one shot trip sources
EALLOW;
EPwm2Regs.TZSEL.bit.OSHT1 = 1;
EPwm2Regs.TZSEL.bit.OSHT2 = 1;

// What do we want the TZ1 and TZ2 to do?
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_HI;
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_HI;

// Enable TZ interrupt
//EPwm2Regs.TZEINT.bit.OST = 1;
EDIS;
#endif


// Setup TBCLK
EPwm2Regs.TBPRD =EPWM2_TIMER_TBPRD; //600; // Set timer period 801 TBCLKs
EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
//EPwm2Regs.TBCTL.bit.PRDLD = 0;


// Set Compare values
EPwm2Regs.CMPA.half.CMPA = EPWM2_MIN_CMPA;//324;//; // Set compare A value
EPwm2Regs.CMPB = EPWM2_MIN_CMPB;//276;//; // Set Compare B value

// Setup counter mode
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
//EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;//0x0-1分频,TBCLK = SYSCLKOUT / (HSPCLKDIV × CLKDIV)

EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Slave module
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through

// Setup shadowing
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

#if 1
// Action Qualifier SubModule Registers
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;//AQ_CLEAR;
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET;//AQ_SET;
EPwm2Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm2Regs.AQCTLB.bit.CBD = AQ_CLEAR;
#endif

#if 1
// Interrupt where we will change the Compare Values
EPwm2Regs.ETSEL.bit.INTSEL = ET_CTRU_CMPB;//ET_CTR_ZERO; // Select INT on Zero event
mPWM2_Disable(); // Disable INT ,close pwm disable,open pwm enable
EPwm2Regs.ETPS.bit.INTPRD = ET_2ND; // Generate INT on 3rd event
#endif

#if 1

EALLOW;
//===========================================================================
// TZA events can force EPWMxA
// TZB events can force EPWMxB
#if 1
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_HI;//硬件反向了 // EPWM1A will go low //故障产生时的保护
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_HI; // EPWM1B will go low
#endif
EPwm2Regs.TZFRC.bit.OST = 1; // Turn off the PWM

EDIS;
#endif

}

  • 你说的有嗒一声是什么器件发出来的,此时PWM的波形是怎么样的?

  • 嗒的一声是线圈盘上发出来的,我们用在电磁加热上面,我用示波器量了PWM驱动波形,发现没有问题。

    我将CMPA与CMPB更改后,如下更改,就在EPwm2Regs.TBPHS.half.TBPHS = 900,再往下减1就有嗒的一声,(EPwm2Regs.TBPHS.half.TBPHS = 810;再往下减1也有嗒的一声),我感觉应该是驱动那个地方配置有问题。

    EPwm1Regs.CMPA.half.CMPA = 900; 
    EPwm1Regs.CMPB = 810; 
    EPwm1Regs.TBPRD = 1580;

    EPwm2Regs.CMPA.half.CMPA = 900; 
    EPwm2Regs.CMPB = 810; 
    EPwm2Regs.TBPRD = 1580;

  • 你把EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
            EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

           EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero

           EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    改成EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; // Load on Zero
            EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;

    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_PRD; // Load on Zero
    EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_PRD;


    试试

  • 按上述方法试了,还是不行。

    后又用高精度示波器抓取了一下,发现在相位切换过程中驱动确实有问题,PWM2的驱动波形如下图,应该是那个地方配置有问题,求解?

  • 补充:

         增加    EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP;

    测试下,在往上加1就有嗒的一声,(EPwm2Regs.TBPHS.half.TBPHS = 835;;再往上加1也有嗒的一声,EPwm2Regs.TBPHS.half.TBPHS = 745,再往上加1也有嗒的一声)

  • 这个问题最后怎么解决的