This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP2812中,如何调用DELAY_US,需要注意什么?需要同时在哪些文件中添加什么语句?



  初学dsp,想要调用dsp自身带的时间延时函数,请各位大神指点一下如何操作,以及需要在工程中添加什么文件等等。

  • 在很多程序中都会调用延时程序DELAY_US(A),在文件DSP281x_Examples.h中有如下宏定义:
    #define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)

    从定义很容易推算出,需要延时A微妙就把DELAY_US()的参数设置为A即可。

    在仿真调试的情况下运行程序,延时是较准确的,但是当把程序烧写到flash里运行时,如果程序上不做修改,就会很容易发现延时的时间比你设置的要长(通过延时控制LED灯闪烁,很直观)。这是因为,DSP访问flash时需要等待时间的,而访问RAM时几乎是零等待,所以在使用DELAY_US(A)时要想延时时间准确必须使其在RAM里运行,在程序上需做如下修改:

    1、在DSP2833x_usDelay.asm中,有如下代码:


           .def _DSP28x_usDelay
           .sect "ramfuncs"

            .global  __DSP28x_usDelay
    _DSP28x_usDelay:
            SUB    ACC,#1
            BF     _DSP28x_usDelay,GEQ    ;; Loop if ACC >= 0
            LRETR

    其中.sect "ramfuncs"语句的作用就是就把用汇编写的函数DSP28x_usDelay定位在ramfuncs段。

  • 我就是把#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)放在了程序里,可是他显示的有错误啊

  • 我就是把#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L)放在了程序里,可是他显示的有错误啊