通过代码生成设置AD采样为差分输入精度16bit,但是在CCS上看没有设置成功,依旧是12bit,为什么?




This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
对于 16 位 ADC 模式:
1. 硬件输入应该是差分的;
2. ADCCTL2 SIGNALMODE =1,分辨率=1;
3. 对于 16 位模式,ADCSOC0CTL ACQPS 是一个较大的数字(对于 200MHz 时钟,可以尝试使用 119)。
详细参考下面的链接