This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320F28335与AD7656通信问题



AD7656通信程序,使用INITF的16位数据方式,其中数据线对应GPIO64~79,RD为149脚XRD,CS为150脚GPIO37,用示波器观察CONVERT和BUSY信号感觉没什么问题了,RD和CS信号也感觉没什么问题了,但是不知道为什么返回数据不太对,而且只有V1和V2的数据返回,请帮忙看一下什么问题,谢谢了。

  • 首先确认一下  数据线和地址线有没有冲突      也就是你的zone*区域只扩展了一片ADC是吗  

    当CS片选时只有一个外设选中吧    有条件的话看看CS等使能信号哦有没有动作