This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 关于DCSM OTP 地址对齐的编程问题

Part Number: TMS320F280049C


你好!

我在使用TMS320F280049C DCSM 的时候,想到了一些问题,请教一下各位工程师,谢谢!

问题1:

DCSM OTP编程必须是128bit地址边界对齐,但是我在CCS使用dcsm_security_tool.syscfg工具配置DCSM的时候,生成的dcsm.asm中有部分地址不是128bit地址对齐的,但实际上是能成功编程DCSM OTP的,请问这是为什么呢?

问题2:

因为对flash/OTP内存编程时,同时需要对其相应的ECC地址进行编程ECC值。

通过FlashAPI 的Fapi_issueProgrammingCommand()函数,使用Fapi_AutoEccGeneration 模式,是可以完成对ECC地址编程的。

但是如果通过CCS使用dcsm_security_tool.syscfg工具配置DCSM的时候,生成的dcsm.asm,直接对DCSM OTP进行编程,却没有对其相应ECC地址编程,请问这正确吗?或者说已经实现了对ECC编程,请告诉我详细情况,可以吗?