This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教永磁同步电机开发套件的两个问题

Other Parts Discussed in Thread: DRV8301

各位老师好,我购买的是28069M和DRV8301组成的永磁同步电机开发套件。有两个问题想请教一下:

1. 在板卡硬件手册的引脚说明上看到有4个PWM_DAC可用,但其中PWM_DAC3并不能正常使用,经过查看示例程序的源码后,发现该引脚GPIO8被设置成ADCSOCAO,如果我将其改回EPWM5,那么ADC转换是不是就不能正常运作了呢?(经实际测试,改动后ADC仍然可用,可能ADCSOCAO仍然在内部起作用的,只是不再输出到外部了吧)

2. 板卡上的电机电流反馈引脚IA_FB,IB_FB,IC_FB都是通过shunt current measurement测得的电流信号,是不是这些引脚信号并不能显示实际的电机电流波形,而是要经过处理后才能得到呢?

谢谢!

  • 1、ADCSOCAO是用来外部启动ad转换的开关,只要不使用外部启动就可以留作他用

    2、不太明白表达的意思,只说采样过程,经过电流传感器变比为较小电流,经采样电阻获得电压信号,然后可以通过运放电路得到可输入ad采样模块的电压,ad采样模块得到的值乘以采样比就是实际电流值

  • 1. 感谢您的回答,因为我在28069的手册上看到ADCSOCAO的I/O类型是作为OUTPUT输出型,所以搞不清到底是什么作用的,这样看来应该是作为INPUT输入型。

    2. 经过实测,IA_FB的波形不是电机电流的正弦波,而是频率接近PWM频率的脉冲波形。说明确实是采用了shunt current measurement,只有在三相逆变桥的低边的开关管开通时,才有电流采样

     

  • DRV8301 手册的确有提到:

    8.3.2 Current Shunt Amplifiers

    The DRV8301 includes two high-performance current shunt amplifiers to accurate low-side, inline current measurement.