导入工程到CCS时,
若选取“Import Legacy CCSv3.3 Project”,则在最后一步即将结束导入时,弹窗:
The directory 'XXX' already contains Eclipse metadata! If the legacy project has already been migrated, import it as a regular CCS project. Otherwise, delete all Eclipse project metadata before migrating.
若选取"Import Existing CCS/CCE Eclipse Project",同样也是在最后一步即将结束导入时,弹窗:
The Managed Make project file could not be read because of the following error:
The Managed Make project file for project SRC_ROOT is missing.
Managed Make functionally will not be available for this project.
请指点一下。我用的是CCS V4.2.0版本,用V4.1.2也试过,同样的弹窗错误提示。请教大家,是版本的问题么?有些地方组要注意的么?谢谢!