This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

导入工程到CCS时弹窗的问题



导入工程到CCS时,

若选取“Import Legacy CCSv3.3 Project”,则在最后一步即将结束导入时,弹窗:

The directory 'XXX' already contains Eclipse metadata! If the legacy project has already been migrated, import it as a regular CCS project. Otherwise, delete all Eclipse project metadata before migrating.

若选取"Import Existing CCS/CCE Eclipse Project",同样也是在最后一步即将结束导入时,弹窗:

The Managed Make project file could not be read because of the following error:
The Managed Make project file for project SRC_ROOT is missing.
Managed Make functionally will not be available for this project.

请指点一下。我用的是CCS V4.2.0版本,用V4.1.2也试过,同样的弹窗错误提示。请教大家,是版本的问题么?有些地方组要注意的么?谢谢!

  • 使用CCSV4的比较少     建议使用V5或V6版本

    import不成功     建议你基于v4建立工程    将源文件添加进来试试

     

  • 我刚刚按照您的方法,基于V4新建了一个project,然后在右键选择“Add files to project”,发现只能一个文件进行添加,不能整个文件夹进行添加。有办法解决这个问题么?

    另外,如果用V5,V6的版本,就可以解决掉导入弹窗的问题了么?

    公司用的是合众达SEED 510plus 驱动器,我查询的结论是:V5.3——V6版本不能兼容这款驱动器。不知其他V5版本的能否兼容呢?谢谢!

  • 重新安装了CCS,这次是V5.1版本,若选取“Import Legacy CCS V3.3 project”,那么,还是会弹出之前一样的窗口错误提示;若选取“Import Existing CCS/CCE Eclipse Project”,那么会弹出:

    Issues that may require your attantion were encountered while importing the project(s).

    Reason:

    See datails below:

    Error: Import failed for project "XXX" because its complier definition is not available. Please install the C2000v6.1 compiler before importing this project.

    看了这个错误弹窗后,我以为可能是安装过程中没有安装C2000v6的编译文件,所以我就在网上搜C2000v6.1的编译器下载链接,然后,安装了这个编译文件。

    接着再打开CCS V5,还是同样的问题。

    接着我开始怀疑是不是C2000v6.1的路径应该放在CCS V5的ccsbase下的C2000文件夹里。于是我照着这样尝试了一遍,还是报一样的错误弹窗。

    请您指点一下,怎样才能避免这种错误弹窗呢?谢谢了!!

  • 你新建工程看看里面是否可以选择到你安装版本的编译器,如果不能,有可能ccs并没有识别

  • changjiang liu 说:

    你新建工程看看里面是否可以选择到你安装版本的编译器,如果不能,有可能ccs并没有识别

    changjiang,你好!

    新建工程只能选择v5.2.6版本的代码生成工具(code generation tool),如下面的截图所示:

    而我目前使用的是v4.2版本,是不是要换成v5.2.6版本的才可以?

  • 建议你下载CCS5.5以上版本,编译器可以在以下链接下载安装http://software-dl.ti.com/codegen/non-esd/downloads/download.htm#C2000

  • 问题解决了!

    有两点可以供后面遇到跟我类似的问题的伙伴们参考:

    1、导入路径不能是桌面,一定要是全英文名路径

    2、勾选“copy projects into workspace”。如下图所示:

    因为我要打开的这个工程是在3.3版本的基础上建立的,而我用的CCS版本是V4.2的,所以通过勾选这个选项,相当于是把原版本的工程转换成V4.2版本兼容的工程。

    可以通过观察workspace文件夹知道:如果不勾选,那么在workspace中不会自动创建一个对应的工程文件夹;如果勾选,那么在workspace中会自动生成一个对应的工程文件夹。

  • 就是这个!感谢!

  • 我的也出现这种弹框,照楼上做法行不行。。。左后我勾选keep original location。。。。反而可以。。可以我work space之前并没有添加过这个工程(查看过work space文件夹确认过)。。。。。希望给后面的人一点参考

  • 我的也是这种情况。另外导入到ccs6.0以后会自动生成一个文件夹,下次再导入时就失败了,要删除那个新生成的文件夹
  • 导入工程时,不要勾选Copy project into workplace。