This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812自带AD采样频率设置



我想用DSP自带的AD进行数据采样,然后现在对采用率有点模糊,通过cputimer定时启动AD可以更改其采样频率,是吧?麻烦您能抽出一点时间,看一下我的程序吗?

程序设置为1s定时器触发一次(这是为了测试,所以频率设置很低),可是理论上AD中断也是1s才对,可实际感觉不对(我在AD中断程序里面放置了 IO口,观察其高低电平变化),每1s定时器触发后,AD要隔4 、5s时间,这是怎么回事?能帮我解答一下吗?谢谢!!

这是定时器 和AD的中断程序,麻烦您看一下,指出问题,好吗?
interrupt void ad(void)
{
    DINT;
  PieCtrl.PIEACK.all=0xffff;
      A0Toggle;//A0端口 高低变化,每次AD采样一次,A0端口变化一次

    adsample1[aa]=AdcRegs.RESULT4>>4;
   aa++;
    if(aa>=100)
 {
    aa=0;
 }    
 //???????????????????????????????????/请问 ,此处下面的设置对吗? AD中断完成后 直接回到主程序的for 还是 cputimer的中断程序??    
  AdcRegs.ADC_ST_FLAG.bit.INT_SEQ1_CLR=1;
 // AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;
// ReloadCpuTimer0();
// StartCpuTimer0();
     // PieCtrl.PIEACK.bit.ACK1 = 1;
  // EINT;
}

interrupt void cpu_timer0_isr(void)
{
    DINT;
 CpuTimer0Regs.TCR.bit.TIF=1;//clear 中断标志
 StopCpuTimer0();
    //A0Toggle;
    while(AdcRegs.ADC_ST_FLAG.bit.SEQ1_BSY==0)  //此处开启AD转换模式
 {   
 AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;
 }
 CpuTimer2.InterruptCount++;
  ReloadCpuTimer0();
 StartCpuTimer0();
 PieCtrl.PIEACK.bit.ACK1 = 1;
 EINT;
}