Other Parts Discussed in Thread: TMS320F28027
请查看附件文档
TMS320F28027之ADC 参考文档SPRUGE5F
TMS320F28027的ADC功能:
1.12位双采样保持电路。
2.同时采样和序列采样方式。
3.全范围电压输入,0V到3.3V固定,或者VREFLO到VREFHI可调。
4.系统时钟全频运行,无需分频。
5.16输入通道。
6.16个SOC配置,设置触发,采样窗口,通道。
7.16个独立保存转换结果的结果寄存器。
8.多触发源。
9.9个灵活的PIE中断。
SOC操作原理: 与以往的ADC类型不同,TMS320F28027的ADC为3型,它是基于SOC的而不是基于序列的。SOC可以配置定义一个单独通道的独立转换。包括三种配置:开始转换的触发源,转换的通道,采样窗口的大小。每个SOC是独立配置的,可以有很多种触发源,通道,采样窗口大小的组合。如果需要,多个SOC可以配置成一样的触发源,通道,采样窗口大小。这提供了一种灵活的配置方法。可以配置转换在不同通道用不同的触发独立采样。可以用一个单独的触发过采样一个相同的通道。可以创建同一个触发不同通道的转换序列。 SOCx的触发源由ADCSOCxCTL寄存器中的TRIGSEL和ADCINTSOCSEL1或 ADCINTSOCSEL2 寄存器配置。软件可以通过ADCSOCFRC1寄存器产生一个SOC事件。通道和采样窗口大小可以通过ADCSOCxCTL寄存器的CHSEL和ACQPS配置。