This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x95c page 0. Available memory ranges: 28027_RAM_lnk.cmd /Example_2802xAdcSoc line 114 C/C++ Problem
图1 是RAM CMD配置文件,
图2 是debug 编译后的map图
请问,从map图中看.txt 占用的孔见是0x6dd,而我给。txt分配的空间是0x900,为什么还说空间不足呢?谢谢解惑!
错误描述:Description Resource Path Location Type
<a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x95c page 0. Available memory ranges: 28027_RAM_lnk.cmd /Example_2802xAdcSoc line 114 C/C++ Problem
我现在按照你的说法把.txt扩展到 0xB00,应该大于0x95C的要求大小了。但是现在还是出现上面的报错,不知道是什么问题?感谢百忙中给予答复!
现在这个问题基本上解决了。谢谢支持!
现在遇到另外一个问题,我用的CCS V5,每次编译后产生的problem信息,更新不了。
比如说,因CMD 空间分配产生的问题,被解决后,理应重新编译后,之前的CMD memory 错误提示应该没有的。
但是错误提示还在那里。除非,将程序 delete后,再重新导入编译。之前的错误提示才消失。
不知道,这个问题怎么解决,谢谢大家帮忙!
谢谢,请问rebuild 选项在哪设置,我的DSP 运行环境是CCS5。谢谢!