This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.2 XDS100 V2 仿真不成功



一个以前的28034的板子做前期仿真调试用,板子确认是好的,以前板子都是用串口烧写的程序,本人在程序DSP280x_CSMPasswords.asm 中设置了密码,现在我自己连上一个JTAGE接口及其电路,用CCS5.2 编译器烧写不进去程序(编译器一直显示Launcning 100%),但经过Test connection 后显示 连接正常: The JTAG IR Integrity scan-test has succeeded。 The JTAG DR Integrity scan-test has succeeded。 尝试过用CCS3.3+xds1000 v1.0 连接,显示也是连接不上。提示我RESET EMULATOR,复位后仍然连不上 不知道会不会是芯片内部密码的原因还是因为外接JTAG电路有问题。 谢谢大家的帮忙分析。