Part Number: TMS320F28335
我的TMS320F28335flash和ram不够用了,想外扩flash和ram,我看别人画的原理图外扩flash和ram接到了同一个接口,这样flash和ram可以同时使用吗?
如果可以同时使用那么和内部flash和ram使用起来有什么区别?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
我的TMS320F28335flash和ram不够用了,想外扩flash和ram,我看别人画的原理图外扩flash和ram接到了同一个接口,这样flash和ram可以同时使用吗?
如果可以同时使用那么和内部flash和ram使用起来有什么区别?
您好,
TMS320F28335可通过XINTF接口使用外部memory,请参考技术手册“Chapter 14"进行连接和配置.
TMS320x2833x, TMS320x2823x Technical Reference Manual (ti.com.cn)
XINTF示例代码请参考 xintf_run_from (ti.com)