This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
我下载了sprc178的程序f2812 PMSM - C2000︎ 微控制器论坛 - C2000 微控制器 - E2E
设计支持 (ti.com) (PMSM3_3).
该项目运行在CCS 7.4,0
我在导入程序后遇到了这个错误
>> Compilation failure makefile:150: recipe for target 'C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out' failed undefined first referenced symbol in file --------- ---------------- _DLOG_4CH_init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _DLOG_4CH_update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_DRIVE_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_DRIVE_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_PWM_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_PWM_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV2_Resolver_PWM_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV2_Resolver_PWM_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_adc04b_drv_init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_adc04b_drv_read C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _clarke_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _ipark_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _park_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _pid_reg3_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _rampgen_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _rmp_cntl_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _svgendq_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out" not built gmake[1]: *** [C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out] Error 1 gmake: *** [all] Error 2 makefile:146: recipe for target 'all' failed **** Build Finished ****
根据这个问题,不确定应该添加哪个库。
看看我的文件搜索路径
Thanks in advance
您好,谢谢您的回复
刚才我按照您的评论加入了库,但事实上我是少加入了.c文件才导致的这个情况,我加入之后错误减少了一些,但是还是存在一些错误
>> Compilation failure makefile:161: recipe for target 'C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out' failed undefined first referenced symbol in file --------- ---------------- _DLOG_4CH_init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _DLOG_4CH_update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_DRIVE_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_DRIVE_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_PWM_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV1_PWM_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV2_Resolver_PWM_Init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_EV2_Resolver_PWM_Update C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_adc04b_drv_init C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _F281X_adc04b_drv_read C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj _svgendq_calc C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/pmsm3_3.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out" not built gmake[1]: *** [C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out] Error 1 gmake: *** [all] Error 2 makefile:157: recipe for target 'all' failed **** Build Finished ****
您好
我上述的问题已经解决了,但是又有一个新的问题,在f281xadc04b.c中
#define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_CLOCK_SPEED) - 9.0L) / 5.0L) extern void DSP28x_usDelay(unsigned long Count);
编译就会报错
>> Compilation failure makefile:182: recipe for target 'C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out' failed undefined first referenced symbol in file --------- ---------------- _DSP28x_usDelay C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/obj/f281xadc04b.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out" not built gmake[1]: *** [C:/tidcs/DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3_281x_CCS3x/../../../../../../../../DMC/c28/v32x/sys/PMSM3_3_281x/cIQmath/build/pmsm3_3.out] Error 1 makefile:178: recipe for target 'all' failed gmake: *** [all] Error 2
但是在281xileg_vdc.c、f281xadc04u.c、f281xileg.c也是相同的代码,就不会报错,请问这是什么原因