Part Number: TMS320F28335
Other Parts Discussed in Thread: TLV320ADC3140
我用TMS320F28335的McBSP读取8个通道的数据,每个通道都是32位,然后用DMA读取到rdata数组中rdata是1024个int32数组。结果我实验的过程中发现,正常读取数据是没有问题的,但是当我中断的时候,就是DMA可以配置接收1024个数据进行中断处理,我把这1024个数据进行了求补码的操作,几个rdata中的数据发生了移位,比如本来是0 1 2 3 4...1027,现在成了2 3 4 5 ...1027 0 1就是向后移了几个顺序,而且顺序一直在变,不是固定的。这样我就没法把每个通道对应的数据取出来了,因为我不知rdata的第几个数据对应的是通道一,那个对应的是通道二,所以这是为什么会发生这样的情况呢,我该怎么解决呢。void init_dma_32()
{
EALLOW;
DmaRegs.DMACTRL.bit.HARDRESET = 1;
asm(" NOP");
// Channel 2, McBSPA Receive
DmaRegs.CH2.BURST_SIZE.all = 1; // 2 words/burst
DmaRegs.CH2.SRC_BURST_STEP = 1; // Increment 1 16-bit addr. btwn words
DmaRegs.CH2.DST_BURST_STEP = 1; // Increment 1 16-bit addr. btwn words
DmaRegs.CH2.TRANSFER_SIZE = 1023; // Interrupt every 63 bursts/transfer
DmaRegs.CH2.SRC_TRANSFER_STEP = 0xFFFF; // Decrement back to DRR2
DmaRegs.CH2.DST_TRANSFER_STEP = 1; // Move to next word in buffer after each word in a burst
DmaRegs.CH2.SRC_ADDR_SHADOW = (Uint32) &McbspaRegs.DRR2.all; // Start address = McBSPA DRR
DmaRegs.CH2.SRC_BEG_ADDR_SHADOW = (Uint32) &McbspaRegs.DRR2.all; // Not needed unless using wrap function
DmaRegs.CH2.DST_ADDR_SHADOW = (Uint32) &rdata[0]; // Start address = Receive buffer (for McBSP-A)
DmaRegs.CH2.DST_BEG_ADDR_SHADOW = (Uint32) &rdata[0]; // Not needed unless using wrap function
DmaRegs.CH2.CONTROL.bit.SYNCCLR = 1; // Clear sync flag
DmaRegs.CH2.CONTROL.bit.ERRCLR = 1; // Clear sync error flag
DmaRegs.CH2.DST_WRAP_SIZE = 1023; // Put to maximum - don't want destination wrap
DmaRegs.CH2.SRC_WRAP_SIZE = 1023; // Put to maximum - don't want source wrap
DmaRegs.CH2.MODE.bit.CHINTE = 1; // Enable channel interrupt
DmaRegs.CH2.MODE.bit.CHINTMODE = 1; // Interrupt at end of transfer
DmaRegs.CH2.MODE.bit.PERINTE = 1; // Enable peripheral interrupt event
DmaRegs.CH2.MODE.bit.PERINTSEL = DMA_MREVTA; // Peripheral interrupt select = McBSP MRSYNCA
DmaRegs.CH2.CONTROL.bit.PERINTCLR = 1; // Clear any spurious interrupt flags
DmaRegs.CH2.MODE.bit.ONESHOT = 0;
EDIS;
}
以上是DMA的配置,因为数据是TLV320ADC3140芯片传过来的,只需要配置接收通道就行。
interrupt void local_DINTCH2_ISR(void) // DMA Ch2
{
/*
Uint16 i;
//原始数据有问题,需要交换高低16位数据,比如0xFFFF0000,需要变为0X0000FFFF
for(i = 0;i<1024;i++)
{
CorrectDATA[i] = ((rdata[i] & 0xFFFF0000) >> 16) | ((rdata[i] & 0x0000FFFF) << 16);
}
for(i = 0;i<128;i++)
{
//x1
if(CorrectDATA[i*8] < 0)
{
x1[i] = ~CorrectDATA[i*8] + 1;
if (x1[i] & 0x8000)//符号位不变,上一步取反把符号位也取反了,这里是还原符号位
{
x1[i] &= 0xefff; // 清除符号位
}
else
{
x1[i] |= 0x8000;
}
}
else
{
x1[i] = CorrectDATA[i*8];
}
//x2
if(CorrectDATA[i*8 + 1] < 0)
{
x2[i] = ~CorrectDATA[i*8 + 1] + 1;
if (x2[i] & 0x8000)//符号位不变,上一步取反把符号位也取反了,这里是还原符号位
{
x2[i] &= 0xefff; // 清除符号位
}
else
{
x2[i] |= 0x8000;
}
}
else
{
x2[i] = CorrectDATA[i*8 + 1];
}
//x3
if(CorrectDATA[i*8 + 2] < 0)
{
x3[i] = ~CorrectDATA[i*8 + 2] + 1;
if (x3[i] & 0x8000)//符号位不变,上一步取反把符号位也取反了,这里是还原符号位
{
x3[i] &= 0xefff; // 清除符号位
}
else
{
x3[i] |= 0x8000;
}
}
else
{
x3[i] = CorrectDATA[i*8 + 2];
}
//x4
if(CorrectDATA[i*8 + 3] < 0)
{
x4[i] = ~CorrectDATA[i*8 + 3] + 1;
if (x4[i] & 0x8000)//符号位不变,上一步取反把符号位也取反了,这里是还原符号位
{
x4[i] &= 0xefff; // 清除符号位
}
else
{
x4[i] |= 0x8000;
}
}
else
{
x4[i] = CorrectDATA[i*8 + 3];
}
}
*/
EALLOW; // NEED TO EXECUTE EALLOW INSIDE ISR !!!
DmaRegs.CH2.CONTROL.bit.RUN = 1; // Re-enable DMA CH2. Should be done every transfer
PieCtrlRegs.PIEACK.all = PIEACK_GROUP7; // To receive more interrupts from this PIE group, acknowledge this interrupt
EDIS;
return;
}
这是DMA的中断服务程序,我把注释掉的程序运行的时候就会出现我所说的情况,如果中断服务程序什么也不做,那数据就是正常的,rdata【0】就是第一个通道rdata【7】就是第八个通道,依次循环。
还请各路豪杰,指点迷津