This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
进行单核SCI数据收发过程时,选择不使用FIFO模式,进行数据收发时,数据读取使用函数SCI_readCharBlockingNonFIFO(SCIA_BASE),将读取到的数据存放在字符串数组中,读取到却是一长串十六进制ascll码,并且只有前两位和7、8位15、16位是正确的,其余都是错误的,我发送的数据是一串带帧头帧尾的数据串,想将这串数据从助手中原封不动收回来,并且设置定时发送可以稳定收到#,101443.00,103.68373212,36.12000077,1510.5636,214.74,-1.27,1,3,40,-0.032,0.011,-0.029,0.068115,0.006653,0.063416,-0.006561,-0.069748,1.001160*,在串口助手中收到的数据截图为,我的代码如下,麻烦指教。
#include "driverlib.h" #include "device.h" #include "RS422.h" #include "string.h" #define SCI_EMPTY 0 #define MAX_DATA_LENGTH 160 char dataString[MAX_DATA_LENGTH]; uint16_t bufferIndex = 0; uint8_t startReading = 0; char send1_flag = 0; void main(void) { uint16_t t = 0; Device_init(); Device_initGPIO(); GPIO_setMasterCore(28, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_28_SCIA_RX); GPIO_setDirectionMode(28, GPIO_DIR_MODE_IN); GPIO_setPadConfig(28, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(28, GPIO_QUAL_ASYNC); GPIO_setMasterCore(29, GPIO_CORE_CPU1); GPIO_setPinConfig(GPIO_29_SCIA_TX); GPIO_setDirectionMode(29, GPIO_DIR_MODE_OUT); GPIO_setPadConfig(29, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(29, GPIO_QUAL_ASYNC); SCI_setConfig(SCIA_BASE, DEVICE_LSPCLK_FREQ, 230400, (SCI_CONFIG_WLEN_8 | SCI_CONFIG_STOP_ONE | SCI_CONFIG_PAR_NONE)); SCI_resetChannels(SCIA_BASE); SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXRDY | SCI_INT_RXRDY_BRKDT); SCI_enableModule(SCIA_BASE); SCI_performSoftwareReset(SCIA_BASE); Interrupt_initModule(); Interrupt_initVectorTable(); SCI_enableInterrupt(SCIA_BASE, (SCI_INT_RXRDY_BRKDT | SCI_INT_TXRDY)); Interrupt_register(INT_SCIA_RX, sciaRXFIFOISR); Interrupt_enable(INT_SCIA_RX); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9); EINT; ERTM; #ifdef AUTOBAUD // // Perform an autobaud lock. // SCI expects an 'a' or 'A' to lock the baud rate. // SCI_lockAutobaud(SCIA_BASE); #endif while(1) { if (send1_flag) { send1_flag = 0; for (t = 0; t < bufferIndex; t++) { if(dataString[t] == 0) { continue; } SCI_writeCharBlockingNonFIFO(SCIA_BASE,dataString[t]); if(dataString[t] == '\0') { dataString[t] = 0; break; } dataString[t] = 0; } } } } __interrupt void sciaRXFIFOISR(void) { uint16_t receivedChar; while (SCI_isDataAvailableNonFIFO(SCIA_BASE) != SCI_EMPTY) { receivedChar = SCI_readCharBlockingNonFIFO(SCIA_BASE); if (receivedChar == '#') { startReading = 1; bufferIndex = 0; dataString[bufferIndex++] = receivedChar; //continue; } if (startReading) { if (receivedChar == '*') { dataString[bufferIndex++] = receivedChar; dataString[bufferIndex++] = '\r'; dataString[bufferIndex++] = '\n'; dataString[bufferIndex] = '\0'; startReading = 0; } if (bufferIndex < MAX_DATA_LENGTH - 3) { dataString[bufferIndex++] = receivedChar; } } } send1_flag = 1; SCI_clearOverflowStatus(SCIA_BASE); SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXRDY_BRKDT); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9); }
您好,
从您的测试数据来看,字符B丢掉了,猜测是接收程序有问题,只来得及处理2个数据。
请只发送一次#ABCD,跟踪接收程序,看收到的数据是否正确。