进行单核SCI数据收发过程时,选择不使用FIFO模式,进行数据收发时,数据读取使用函数SCI_readCharBlockingNonFIFO(SCIA_BASE),将读取到的数据存放在字符串数组中,读取到却是一长串十六进制ascll码,并且只有前两位和7、8位15、16位是正确的,其余都是错误的,我发送的数据是一串带帧头帧尾的数据串,想将这串数据从助手中原封不动收回来,并且设置定时发送可以稳定收到#,101443.00,103.68373212,36.12000077,1510.5636,214.74,-1.27,1,3,40,-0.032,0.011,-0.029,0.068115,0.006653,0.063416,-0.006561,-0.069748,1.001160*,在串口助手中收到的数据截图为,我的代码如下,麻烦指教。