This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用官方的LAUNCHXL-F280049C开发板,跑adc_ex1_soc_software例程验证ADC采样的问题顶,我在while(1)循环中把最后的ESTOP0屏蔽,然后在线调试,观察myADC0Result0的数值变化,给开发板的A0通道接入了信号源,给1V,发现转换结果在1200-1300之间跳变,数据很不准确,想问下是什么原因?
//############################################################################# // // FILE: adc_ex1_soc_software.c // // TITLE: ADC Software Triggering // //! \addtogroup driver_example_list //! <h1>ADC Software Triggering</h1> //! //! This example converts some voltages on ADCA and ADCC based on a software //! trigger. //! //! The ADCC will not convert until ADCA is complete, so the ADCs will not run //! asynchronously. However, this is much less efficient than allowing the ADCs //! to convert synchronously in parallel (for example, by using an ePWM //! trigger). //! //! \b External \b Connections \n //! - A0, A1, C2, and C3 should be connected to signals to convert //! //! \b Watch \b Variables \n //! - \b myADC0Result0 - Digital representation of the voltage on pin A0 //! - \b myADC0Result1 - Digital representation of the voltage on pin A1 //! - \b myADC1Result0 - Digital representation of the voltage on pin C2 //! - \b myADC1Result1 - Digital representation of the voltage on pin C3 //! // //############################################################################# // // // $Copyright: // Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // // Included Files // #include "driverlib.h" #include "device.h" #include "board.h" // // Globals // uint16_t myADC0Result0; uint16_t myADC0Result1; uint16_t myADC1Result0; uint16_t myADC1Result1; // // Main // void main(void) { // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pullups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Set up ADCs, initializing the SOCs to be triggered by software // Board_init(); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Loop indefinitely // while(1) { // // Convert, wait for completion, and store results // ADC_forceMultipleSOC(myADC0_BASE, (ADC_FORCE_SOC0 | ADC_FORCE_SOC1)); // // Wait for ADCA to complete, then acknowledge flag // while(ADC_getInterruptStatus(myADC0_BASE, ADC_INT_NUMBER1) == false) { } ADC_clearInterruptStatus(myADC0_BASE, ADC_INT_NUMBER1); ADC_forceMultipleSOC(myADC1_BASE, (ADC_FORCE_SOC0 | ADC_FORCE_SOC1)); // // Wait for ADCC to complete, then acknowledge flag // while(ADC_getInterruptStatus(myADC1_BASE, ADC_INT_NUMBER1) == false) { } ADC_clearInterruptStatus(myADC1_BASE, ADC_INT_NUMBER1); // // Store results // myADC0Result0 = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER0); myADC0Result1 = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER1); myADC1Result0 = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER0); myADC1Result1 = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER1); DEVICE_DELAY_US(100); // // Software breakpoint. At this point, conversion results are stored in // myADC0Result0, myADC0Result1, myADC1Result0, and myADC1Result1. // // Hit run again to get updated conversions. // //ESTOP0; } }
您好
这里有几个可能的原因和解决方案供你参考:
参考电压和分辨率问题:
1V / 3.3V * 4096
(假设参考电压为3.3V且分辨率为12位)的计数值,即约1241。信号源和输入通道问题:
ADC校准和偏移:
噪声和干扰:
代码和配置问题:
为了更具体地诊断问题,你可以尝试以下步骤:
非常感谢您的解答,我这边情况是这样的,设计了一款基于TMS320F280049C的电源板,ADC这边数值跳动很大,大约波动有100左右,相对于12位ADC波动达到了2.5%,所以就回过头去看官方的开发板,发现用开发板跑官方例程,用信号源直接给信号的形式波动也比较大,今天又试了将模拟输入引脚短接到开发板的地和VREFHI,波动会小一点,但是也达到了10左右,相当于12位ad只能做到9位左右稳定度,想问下,这个片内的AD理论上能做到多高的稳定度,先不谈精度了?
您好
这是影响单片机内部ADC稳定的相关因素,建议您通过上述建议优化。