This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
does uniflash software support programming 2 dsp chip via JTAG? These 2 chip serial connect through JTAG.
current I can burn the 2 standalone dsp like 28335 via CCS.
but once using uniflash, I can see only one processor.
So is there any special setting required?
Regards
Dragon
I did below setting in the ccxml file.
now I can use uniflash program 28388d and by pass the 1st processor 280025. similar setting when program the 280025.