Part Number: TMS320F28035
ADCSOC使用顺序采样,采样频率为70KHz。
当SOC0通道进行切换的时候,例如SOC0,1s采样ADCINA1,1s采样ADCINB4,这样操作为什么会影响到其他通道的采样?
例如:

但有时候又不会有影响,例如SOC,在ADCINA1和ADCINB7,之间行进切换
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
ADCSOC使用顺序采样,采样频率为70KHz。
当SOC0通道进行切换的时候,例如SOC0,1s采样ADCINA1,1s采样ADCINB4,这样操作为什么会影响到其他通道的采样?
例如:

但有时候又不会有影响,例如SOC,在ADCINA1和ADCINB7,之间行进切换
您好,
SOC的触发源一样的吗?
在TRM中“8.2 SOC Principle of Operation”有SOC使用的应用示例,确定符合您应用的案例。
TMS320F2803x Microcontrollers Technical Reference Manual (Rev. A)
同时请参考示例代码Example_2803xAdcSoc.c
您好,
可能你还没理解我的问题,并不是ADC采样不能正常触发,而是使用pwm周期(70Khz)触发ADC采样,采样数值正常,以上都没有问题,但我想实现的是SOC0,1s采样ADCINA1,1s采样ADCINB4,即一个soc采两个ADC
初始化代码:
void InitAdc(void)
{
// *IMPORTANT*
// The Device_cal function, which copies the ADC calibration values from TI reserved
// OTP into the ADCREFSEL and ADCOFFTRIM registers, occurs automatically in the
// Boot ROM. If the boot ROM code is bypassed during the debug process, the
// following function MUST be called for the ADC to function according
// to specification. The clocks to the ADC MUST be enabled before calling this
// function.
// See the device data manual and/or the ADC Reference
// Manual for more information.
EALLOW;
SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
(*Device_cal)();
EDIS;
// To powerup the ADC the ADCENCLK bit should be set first to enable
// clocks, followed by powering up the bandgap, reference circuitry, and ADC core.
// Before the first conversion is performed a 5ms delay must be observed
// after power up to give all analog circuits time to power up and settle
// Please note that for the delay function below to operate correctly the
// CPU_RATE define statement in the DSP2803x_Examples.h file must
// contain the correct CPU clock period in nanoseconds.
EALLOW;
AdcRegs.ADCCTL1.bit.ADCREFSEL = 1; // Select external BG
AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Power ADC BG
AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; // Power reference
AdcRegs.ADCCTL1.bit.ADCPWDN = 1; // Power ADC
AdcRegs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Overlap of sample is not allowed
AdcRegs.ADCCTL2.bit.CLKDIV2EN = 0; // 0 :ADC clock = CPU clock //1: ADC clock = CPU clock/2
AdcRegs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC
EDIS;
DELAY_US_APP(ADC_usDELAY);
AdcOffsetSelfCal();
EALLOW;
AdcRegs.ADCCTL1.bit.ADCREFSEL = 1; // Select external BG
AdcRegs.ADCSAMPLEMODE.all = 0; // Single sample mode
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC0CTL.bit.CHSEL = ADCASOC0;
AdcRegs.ADCSOC0CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC1CTL.bit.CHSEL = ADCASOC1;
AdcRegs.ADCSOC1CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC2CTL.bit.CHSEL = ADCASOC2;
AdcRegs.ADCSOC2CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC3CTL.bit.CHSEL = ADCASOC3;
AdcRegs.ADCSOC3CTL.bit.ACQPS = 0xA;
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC4CTL.bit.CHSEL = ADCASOC4;
AdcRegs.ADCSOC4CTL.bit.ACQPS = SAMPLE_WINDOW;//0x10;
AdcRegs.ADCSOC5CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC5CTL.bit.CHSEL = ADCASOC5;
AdcRegs.ADCSOC5CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC6CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC6CTL.bit.CHSEL = ADCASOC6;
AdcRegs.ADCSOC6CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC7CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC7CTL.bit.CHSEL = ADCASOC7;
AdcRegs.ADCSOC7CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC8CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC8CTL.bit.CHSEL = ADCASOC8;
AdcRegs.ADCSOC8CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC9CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC9CTL.bit.CHSEL = ADCASOC9;
AdcRegs.ADCSOC9CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC10CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC10CTL.bit.CHSEL = ADCASOC10;
AdcRegs.ADCSOC10CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC11CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC11CTL.bit.CHSEL = ADCASOC11;
AdcRegs.ADCSOC11CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC12CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC12CTL.bit.CHSEL = ADCASOC12;
AdcRegs.ADCSOC12CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC13CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC13CTL.bit.CHSEL = ADCASOC13;
AdcRegs.ADCSOC13CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC14CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC14CTL.bit.CHSEL = ADCASOC14;
AdcRegs.ADCSOC14CTL.bit.ACQPS = SAMPLE_WINDOW;
AdcRegs.ADCSOC15CTL.bit.TRIGSEL = SAMP_TRIG;
AdcRegs.ADCSOC15CTL.bit.CHSEL = ADCASOC15;
AdcRegs.ADCSOC15CTL.bit.ACQPS = TDSP_WINDOW;
AdcRegs.SOCPRICTL.bit.SOCPRIORITY = SAME_PRIORITY;
AdcRegs.ADCCTL1.bit.VREFLOCONV = 1; //Select VREFLO connection on B5
//round cycle ???
// AdcRegs.SOCPRICTL.bit.RRPOINTER = 0x0F;
EDIS;
}