This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: AdcRegs.ADCSOCxxCTL.bit.CHSEL 在运行过程中,进行2s为周期的通道切换,为什么会影响到其他SOC通道?

Part Number: TMS320F28035

ADCSOC使用顺序采样,采样频率为70KHz。

当SOC0通道进行切换的时候,例如SOC0,1s采样ADCINA1,1s采样ADCINB4,这样操作为什么会影响到其他通道的采样?

例如:

但有时候又不会有影响,例如SOC,在ADCINA1和ADCINB7,之间行进切换

  • 您好,

          SOC的触发源一样的吗?

          在TRM中“8.2 SOC Principle of Operation”有SOC使用的应用示例,确定符合您应用的案例。

          TMS320F2803x Microcontrollers Technical Reference Manual (Rev. A)

          同时请参考示例代码Example_2803xAdcSoc.c

  • 您好,

    SOC的触发源是一样。

    示例代码中展示的是在采样前初始化就配置好了SOC的CHSEL,并没有在ADC采样过程中进行切换CHSEL。

  • 您好,

           对于您的应用,建议参考TRM中方法配置。

           

  • 您好,

    可能你还没理解我的问题,并不是ADC采样不能正常触发,而是使用pwm周期(70Khz)触发ADC采样,采样数值正常,以上都没有问题,但我想实现的是SOC0,1s采样ADCINA1,1s采样ADCINB4,即一个soc采两个ADC

    初始化代码:

    void InitAdc(void)
    {

    // *IMPORTANT*
    // The Device_cal function, which copies the ADC calibration values from TI reserved
    // OTP into the ADCREFSEL and ADCOFFTRIM registers, occurs automatically in the
    // Boot ROM. If the boot ROM code is bypassed during the debug process, the
    // following function MUST be called for the ADC to function according
    // to specification. The clocks to the ADC MUST be enabled before calling this
    // function.
    // See the device data manual and/or the ADC Reference
    // Manual for more information.
    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.ADCENCLK = 1;
    (*Device_cal)();
    EDIS;

    // To powerup the ADC the ADCENCLK bit should be set first to enable
    // clocks, followed by powering up the bandgap, reference circuitry, and ADC core.
    // Before the first conversion is performed a 5ms delay must be observed
    // after power up to give all analog circuits time to power up and settle

    // Please note that for the delay function below to operate correctly the
    // CPU_RATE define statement in the DSP2803x_Examples.h file must
    // contain the correct CPU clock period in nanoseconds.

    EALLOW;
    AdcRegs.ADCCTL1.bit.ADCREFSEL = 1; // Select external BG
    AdcRegs.ADCCTL1.bit.ADCBGPWD = 1; // Power ADC BG
    AdcRegs.ADCCTL1.bit.ADCREFPWD = 1; // Power reference
    AdcRegs.ADCCTL1.bit.ADCPWDN = 1; // Power ADC

    AdcRegs.ADCCTL2.bit.ADCNONOVERLAP = 1; // Overlap of sample is not allowed
    AdcRegs.ADCCTL2.bit.CLKDIV2EN = 0; // 0 :ADC clock = CPU clock //1: ADC clock = CPU clock/2

    AdcRegs.ADCCTL1.bit.ADCENABLE = 1; // Enable ADC
    EDIS;

    DELAY_US_APP(ADC_usDELAY);

    AdcOffsetSelfCal();

    EALLOW;
    AdcRegs.ADCCTL1.bit.ADCREFSEL = 1; // Select external BG
    AdcRegs.ADCSAMPLEMODE.all = 0; // Single sample mode

    AdcRegs.ADCSOC0CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC0CTL.bit.CHSEL = ADCASOC0;
    AdcRegs.ADCSOC0CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC1CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC1CTL.bit.CHSEL = ADCASOC1;
    AdcRegs.ADCSOC1CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC2CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC2CTL.bit.CHSEL = ADCASOC2;
    AdcRegs.ADCSOC2CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC3CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC3CTL.bit.CHSEL = ADCASOC3;
    AdcRegs.ADCSOC3CTL.bit.ACQPS = 0xA;

    AdcRegs.ADCSOC4CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC4CTL.bit.CHSEL = ADCASOC4;
    AdcRegs.ADCSOC4CTL.bit.ACQPS = SAMPLE_WINDOW;//0x10;

    AdcRegs.ADCSOC5CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC5CTL.bit.CHSEL = ADCASOC5;
    AdcRegs.ADCSOC5CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC6CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC6CTL.bit.CHSEL = ADCASOC6;
    AdcRegs.ADCSOC6CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC7CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC7CTL.bit.CHSEL = ADCASOC7;
    AdcRegs.ADCSOC7CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC8CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC8CTL.bit.CHSEL = ADCASOC8;
    AdcRegs.ADCSOC8CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC9CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC9CTL.bit.CHSEL = ADCASOC9;
    AdcRegs.ADCSOC9CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC10CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC10CTL.bit.CHSEL = ADCASOC10;
    AdcRegs.ADCSOC10CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC11CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC11CTL.bit.CHSEL = ADCASOC11;
    AdcRegs.ADCSOC11CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC12CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC12CTL.bit.CHSEL = ADCASOC12;
    AdcRegs.ADCSOC12CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC13CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC13CTL.bit.CHSEL = ADCASOC13;
    AdcRegs.ADCSOC13CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC14CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC14CTL.bit.CHSEL = ADCASOC14;
    AdcRegs.ADCSOC14CTL.bit.ACQPS = SAMPLE_WINDOW;

    AdcRegs.ADCSOC15CTL.bit.TRIGSEL = SAMP_TRIG;
    AdcRegs.ADCSOC15CTL.bit.CHSEL = ADCASOC15;
    AdcRegs.ADCSOC15CTL.bit.ACQPS = TDSP_WINDOW;

    AdcRegs.SOCPRICTL.bit.SOCPRIORITY = SAME_PRIORITY;

    AdcRegs.ADCCTL1.bit.VREFLOCONV = 1; //Select VREFLO connection on B5

    //round cycle ???
    // AdcRegs.SOCPRICTL.bit.RRPOINTER = 0x0F;
    EDIS;
    }

  • 您好,

         请详细描述是如何影响其他通道的采样的。

  • 只有B00地址,即SOC0进行通道切换,但其他通道也受到了影响,影响程序各不相同,


  • 您好,

          请参考链接中的文档。看起来它们可能会受到内存串扰的影响。

          Methods for Mitigating ADC Memory Cross-Talk (Rev. A)