This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P659DK-Q1: TMS320F28P659DK-Q1

Part Number: TMS320F28P659DK-Q1



i want to design a SPI which  can communicate with multiple slaves(for exampel 4).thus there should be 4 chip select signals, but i see in this doc the spiA channle SPIA_PTE can be tied to 13,43, 56, so how can i finish expected 4 slaves communication, i mean can i use a gpio to act as a ship slect signal? or SPIA just could communicate with 3 slaves or just one?
thanks.