This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用示波器测试了pwmA2(黄色)和pwmB2(绿色)引脚,配置的是pwmA2为高电平,pwmB2为低电平,发现pwmA2(黄色)和pwmB2(绿色)开始有三次高低电平翻转(并且死区和我配置的死区时间是一致的),翻转后pwmA2为高电平,pwmB2为低电平,请问为什么上电后有高低电平翻转,需要配置什么才能把这个现象清除。
并且不只是pwmA2和pwmB2有这个现象,pwmA1和pwmB1,pwmA3和pwmB3同样有此现象。
您好,这是我的配置,请帮忙看一下是否配置正确,谢谢。
*在PCLKCR1寄存器中启用ePWM模块时钟。
•将TBCLKSYNC设置为0。
•配置预分频器值和ePWM模式。
•将TBCLKSYNC设置为1
DSP2833x_SysCtrl.c文件
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; // Disable TBCLK within the ePWM
SysCtrlRegs.PCLKCR1.bit.EPWM1ENCLK = 1; // ePWM1
SysCtrlRegs.PCLKCR1.bit.EPWM2ENCLK = 1; // ePWM2
SysCtrlRegs.PCLKCR1.bit.EPWM3ENCLK = 1; // ePWM3
SysCtrlRegs.PCLKCR1.bit.EPWM4ENCLK = 1; // ePWM4
SysCtrlRegs.PCLKCR1.bit.EPWM5ENCLK = 1; // ePWM5
SysCtrlRegs.PCLKCR1.bit.EPWM6ENCLK = 1; // ePWM6
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; // Enable TBCLK within the ePWM
DSP2833x_EPwm.c文件
//###########################################################################
//
// FILE: DSP2833x_EPwm.c
//
// TITLE: DSP2833x ePWM Initialization & Support Functions.
//
//###########################################################################
// $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $
// $Release Date: November 1, 2016 $
// $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
//
// Included Files
//
#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File
#include "ProjectConfig.h"
//
// InitEPwm - This function initializes the ePWM(s) to a known state.
//
void
InitEPwm(void)
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
InitEPwm1();
InitEPwm2();
InitEPwm3();
InitEPwm4();
InitEPwm5();
InitEPwm6();
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
}
//
// InitEPwmGpio - This function initializes GPIO pins to function as ePWM pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
void
InitEPwmGpio(void)
{
InitEPwm1Gpio();
InitEPwm2Gpio();
InitEPwm3Gpio();
InitEPwm4Gpio();
InitEPwm5Gpio();
InitEPwm6Gpio();
}
//
// InitEPwm1Gpio - This function initializes GPIO pins to function as ePWM1
//
void
InitEPwm1Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 0; // Enable pull-up on GPIO0 (EPWM1A)
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pull-up on GPIO1 (EPWM1B)
//
// Configure ePWM-1 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM1 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // Configure GPIO0 as EPWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // Configure GPIO1 as EPWM1B
EDIS;
}
//
// InitEPwm2Gpio - This function initializes GPIO pins to function as ePWM2
//
void
InitEPwm2Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO2 = 0; // Enable pull-up on GPIO2 (EPWM2A)
GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pull-up on GPIO3 (EPWM3B)
//
// Configure ePWM-2 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM2 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // Configure GPIO2 as EPWM2A
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // Configure GPIO3 as EPWM2B
EDIS;
}
//
// InitEPwm3Gpio - This function initializes GPIO pins to function as ePWM3
//
void
InitEPwm3Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO4 = 0; // Enable pull-up on GPIO4 (EPWM3A)
GpioCtrlRegs.GPAPUD.bit.GPIO5 = 0; // Enable pull-up on GPIO5 (EPWM3B)
//
// Configure ePWM-3 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM3 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // Configure GPIO4 as EPWM3A
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // Configure GPIO5 as EPWM3B
EDIS;
}
#if DSP28_EPWM4
//
// InitEPwm4Gpio - This function initializes GPIO pins to function as ePWM4
//
void
InitEPwm4Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; // Enable pull-up on GPIO6 (EPWM4A)
GpioCtrlRegs.GPAPUD.bit.GPIO7 = 0; // Enable pull-up on GPIO7 (EPWM4B)
//
// Configure ePWM-4 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM4 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; // Configure GPIO6 as EPWM4A
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; // Configure GPIO7 as EPWM4B
EDIS;
}
#endif // endif DSP28_EPWM4
#if DSP28_EPWM5
//
// InitEPwm5Gpio - This function initializes GPIO pins to function as ePWM5
//
void
InitEPwm5Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO8 = 0; // Enable pull-up on GPIO8 (EPWM5A)
GpioCtrlRegs.GPAPUD.bit.GPIO9 = 0; // Enable pull-up on GPIO9 (EPWM5B)
//
// Configure ePWM-5 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM5 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; // Configure GPIO8 as EPWM5A
GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; // Configure GPIO9 as EPWM5B
EDIS;
}
#endif // endif DSP28_EPWM5
#if DSP28_EPWM6
//
// InitEPwm6Gpio - This function initializes GPIO pins to function as ePWM6
//
void
InitEPwm6Gpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO10 = 0; // Enable pull-up on GPIO10 (EPWM6A)
GpioCtrlRegs.GPAPUD.bit.GPIO11 = 0; // Enable pull-up on GPIO11 (EPWM6B)
//
// Configure ePWM-6 pins using GPIO regs
// This specifies which of the possible GPIO pins will be ePWM6 functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; // Configure GPIO10 as EPWM6A
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; // Configure GPIO11 as EPWM6B
EDIS;
}
#endif // endif DSP28_EPWM6
//
// InitEPwmSyncGpio - This function initializes GPIO pins to function as ePWM
// Synch pins
//
void
InitEPwmSyncGpio(void)
{
EALLOW;
//
// Configure EPWMSYNCI
//
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; //Enable pull-up on GPIO6 (EPWMSYNCI)
//GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;//Enable pull-up on GPIO32 (EPWMSYNCI)
//
// Set qualification for selected pins to asynch only
// This will select synch to SYSCLKOUT for the selected pins.
// Comment out other unwanted lines.
//
//
// Synch to SYSCLKOUT GPIO6 (EPWMSYNCI)
//
GpioCtrlRegs.GPAQSEL1.bit.GPIO6 = 0;
//
//Synch to SYSCLKOUT GPIO32 (EPWMSYNCI)
//
//GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 0;
//
// Configure EPwmSync pins using GPIO regs
// This specifies which of the possible GPIO pins will be EPwmSync
// functional pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 2; //Enable pull-up on GPIO6(EPWMSYNCI)
//GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 2;//Enable pull-up on GPIO32(EPWMSYNCI)
//
// Configure EPWMSYNC0
//
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
//
// Enable pull-up on GPIO6 (EPWMSYNC0)
//
//GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0;
//
// Enable pull-up on GPIO33 (EPWMSYNC0)
//
GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;
//
// Enable pull-up on GPIO6 (EPWMSYNC0)
//
//GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 3;
//
// Enable pull-up on GPIO33 (EPWMSYNC0)
//
GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 2;
}
//
// InitTzGpio - This function initializes GPIO pins to function as Trip Zone
// (TZ) pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
void
InitTzGpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (TZ1)
GpioCtrlRegs.GPAPUD.bit.GPIO13 = 0; // Enable pull-up on GPIO13 (TZ2)
GpioCtrlRegs.GPAPUD.bit.GPIO14 = 0; // Enable pull-up on GPIO14 (TZ3)
GpioCtrlRegs.GPAPUD.bit.GPIO15 = 0; // Enable pull-up on GPIO15 (TZ4)
GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pull-up on GPIO16 (TZ5)
//GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pull-up on GPIO28 (TZ5)
GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0; // Enable pull-up on GPIO17 (TZ6)
//GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; // Enable pull-up on GPIO29 (TZ6)
//
// Set qualification for selected pins to asynch only
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // Asynch input GPIO12 (TZ1)
GpioCtrlRegs.GPAQSEL1.bit.GPIO13 = 3; // Asynch input GPIO13 (TZ2)
GpioCtrlRegs.GPAQSEL1.bit.GPIO14 = 3; // Asynch input GPIO14 (TZ3)
GpioCtrlRegs.GPAQSEL1.bit.GPIO15 = 3; // Asynch input GPIO15 (TZ4)
GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (TZ5)
//GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (TZ5)
GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // Asynch input GPIO17 (TZ6)
//GpioCtrlRegs.GPAQSEL2.bit.GPIO29 = 3; // Asynch input GPIO29 (TZ6)
//
// Configure TZ pins using GPIO regs
// This specifies which of the possible GPIO pins will be TZ functional
// pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 1; // Configure GPIO12 as TZ1
GpioCtrlRegs.GPAMUX1.bit.GPIO13 = 1; // Configure GPIO13 as TZ2
GpioCtrlRegs.GPAMUX1.bit.GPIO14 = 1; // Configure GPIO14 as TZ3
GpioCtrlRegs.GPAMUX1.bit.GPIO15 = 1; // Configure GPIO15 as TZ4
GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 3; // Configure GPIO16 as TZ5
//GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 3; // Configure GPIO28 as TZ5
GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 3; // Configure GPIO17 as TZ6
//GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 3; // Configure GPIO29 as TZ6
EDIS;
}
//---------------------------------------------------------------------------
// Example: InitEPwm:
//---------------------------------------------------------------------------
void InitEPwm1(void)
{
EPwm1Regs.TBPRD =PWM_PERIOD;// Set timer period 16KHz
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm1Regs.CMPA.half.CMPA = EPwm1Regs.TBPRD>>1; //0% Duty EPwm1Regs.TBPRD*0.8
EPwm1Regs.CMPB = EPwm1Regs.CMPA.half.CMPA; //50% Duty
// Setup TBCLK
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm1Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
// EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; //0:影子模式; 1:立即模式
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; //计数寄存器CTR=0是装载新的比较值
// Set actions
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
// Active Low PWMs - Setup Deadband
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
// 设置ePWM中断生成
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // 在计数为零的时候生成中断事件
EPwm1Regs.ETSEL.bit.INTEN = 1; // 使能中断
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // 每个事件生成中断,选择INTCNT和INTPRD作为事件判断标志
// 设置ePWM的SOCA的生成
EPwm1Regs.ETSEL.bit.SOCAEN = 1; //
EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO; //等于PRD时触发启动转换ADC脉冲,上桥臂关闭中间采样 ET_CTR_PRD
EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; //电流环16KHz ET_1ST
EPwm1Regs.ETCLR.bit.SOCA = 1; //Clear SOCA flag
}
void InitEPwm2(void)
{
EPwm2Regs.TBPRD = EPwm1Regs.TBPRD;
EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm2Regs.CMPA.half.CMPA = EPwm2Regs.TBPRD>>1; //EPwm2Regs.TBPRD; //0% Duty
EPwm2Regs.CMPB = EPwm2Regs.CMPA.half.CMPA; //0% Duty
// Setup TBCLK
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
// EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
// Set actions
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
}
void InitEPwm3(void)
{
EPwm3Regs.TBPRD = EPwm1Regs.TBPRD;// Set timer period 20KHz=80/4000
EPwm3Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm3Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm3Regs.CMPA.half.CMPA = EPwm3Regs.TBPRD>>1; //50% Duty
EPwm3Regs.CMPB = EPwm3Regs.CMPA.half.CMPA; //50% Duty
// Setup TBCLK
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm3Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
// EPwm3Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
// Set actions
EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EALLOW;
//保护设置
EPwm3Regs.TZSEL.bit.CBC3 = TZ_ENABLE; //过流保护触发 cycle by cycle
EPwm3Regs.TZCTL.bit.TZA = TZ_FORCE_LO; //过流时PWMA输出高阻 TZ_HIZ
EPwm3Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //过流时PWMB输出高阻 TZ_HIZ
EPwm3Regs.TZEINT.bit.CBC=1;
EPwm3Regs.TZCLR.all = 0; //清除所有中断标志
EDIS;
}
void InitEPwm4(void)
{
EPwm4Regs.TBPRD =EPwm1Regs.TBPRD;// Set timer period 16KHz
EPwm4Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm4Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm4Regs.CMPA.half.CMPA = EPwm4Regs.TBPRD>>1; //50% Duty EPwm1Regs.TBPRD*0.8
EPwm4Regs.CMPB = EPwm4Regs.CMPA.half.CMPA; //50% Duty
// Setup TBCLK
EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm4Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm4Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; //0:影子模式; 1:立即模式
EPwm4Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm4Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; //计数寄存器CTR=0是装载新的比较值
// Set actions
EPwm4Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm4Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm4Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm4Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm4Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EALLOW;
//保护设置 TZ4触发保护
EPwm4Regs.TZSEL.bit.CBC4 = TZ_ENABLE; //过流保护触发 cycle by cycle
EPwm4Regs.TZCTL.bit.TZA = TZ_FORCE_LO; //过流时PWMA输出高阻 TZ_HIZ
EPwm4Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //过流时PWMB输出高阻 TZ_HIZ
EPwm4Regs.TZEINT.bit.CBC=1;
EPwm4Regs.TZCLR.all = 0; //清除所有中断标志
EDIS;
}
void InitEPwm5(void)
{
EPwm5Regs.TBPRD = EPwm1Regs.TBPRD;// Set timer period 20KHz=80/4000
EPwm5Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm5Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm5Regs.CMPA.half.CMPA = EPwm5Regs.TBPRD>>1; //50% Duty
EPwm5Regs.CMPB = EPwm5Regs.CMPA.half.CMPA; //50% Duty
// Setup TBCLK
EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm5Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm5Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm5Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm5Regs.TBCTL.bit.CLKDIV = TB_DIV1;
// EPwm5Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm5Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm5Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm5Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
// Set actions
EPwm5Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm5Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm5Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm5Regs.DBCTL.bit.IN_MODE = DBA_ALL;
// EPwm5Regs.DBCTL.bit.IN_MODE = DBA_ALL; //输入都是PWMA
// EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //B路不取反 IRS2103 负逻辑
// EPwm5Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //
//
// EPwm5Regs.DBRED = Dead_Time; //死区时间1us
// EPwm5Regs.DBFED = Dead_Time;
EALLOW;
//保护设置 TZ4触发保护
EPwm5Regs.TZSEL.bit.CBC4 = TZ_ENABLE; //过流保护触发 cycle by cycle
EPwm5Regs.TZCTL.bit.TZA = TZ_FORCE_LO; //过流时PWMA输出高阻 TZ_HIZ
EPwm5Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //过流时PWMB输出高阻 TZ_HIZ
EPwm5Regs.TZEINT.bit.CBC=1;
EPwm5Regs.TZCLR.all = 0;
EDIS;
}
void InitEPwm6(void)
{
EPwm6Regs.TBPRD = EPwm1Regs.TBPRD;// Set timer period 20KHz=80/4000
EPwm6Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm6Regs.TBCTR = 0x0000; // Clear counter
// Setup compare
EPwm6Regs.CMPA.half.CMPA = EPwm6Regs.TBPRD>>1; //50% Duty
EPwm6Regs.CMPB = EPwm6Regs.CMPA.half.CMPA; //50% Duty
// Setup TBCLK
EPwm6Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm6Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Disable phase loading
EPwm6Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;
EPwm6Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm6Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm6Regs.TBCTL.bit.CLKDIV = TB_DIV1;
// EPwm6Regs.TBCTL.bit.PHSDIR = TB_UP;
EPwm6Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // Load registers every ZERO or PRD
EPwm6Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm6Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm6Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
// Set actions
EPwm6Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A 斩波
EPwm6Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm6Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm6Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm6Regs.DBCTL.bit.IN_MODE = DBA_ALL;
// EPwm6Regs.DBCTL.bit.IN_MODE = DBA_ALL; //输入都是PWMA
// EPwm6Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; //B路不取反 IRS2103 负逻辑
// EPwm6Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; //
//
// EPwm6Regs.DBRED = Dead_Time; //死区时间1us
// EPwm6Regs.DBFED = Dead_Time;
EALLOW;
//保护设置 TZ4触发保护
EPwm6Regs.TZSEL.bit.CBC4 = TZ_ENABLE; //过流保护触发 cycle by cycle
EPwm6Regs.TZCTL.bit.TZA = TZ_FORCE_LO; //过流时PWMA输出高阻 TZ_HIZ
EPwm6Regs.TZCTL.bit.TZB = TZ_FORCE_LO; //过流时PWMB输出高阻 TZ_HIZ
EPwm6Regs.TZEINT.bit.CBC=1;
EPwm6Regs.TZCLR.all = 0;
//清除所有中断标志
EDIS;
}
//
// End of file
//