Part Number: TMS320F28377D
我使用
Fapi_doMarginRead函数读取flash中含有“0”的数据时发现会出现这一个word中出现某个bit被异常置为1的情况
我是使用读取函数读取了100个字放到ram中,和memory browser窗口中监控到的数据做对比


我使用的代码是这样的

但是使用直接取地址的方式,一个字一个字的读取好像就没问题,希望能得到你们的帮助,非常感谢。
我已经上传了cmd文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
我使用



MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000123, length = 0x0002DD
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x002000
/* RAMLS1 : origin = 0x008800, length = 0x000800*/
/* RAMLS2 : origin = 0x009000, length = 0x000800 */
/* RAMLS3 : origin = 0x009800, length = 0x000800 */
RAMLS4 : origin = 0x00A000, length = 0x001000
//RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
// RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x003FFE /* on-chip Flash */
//FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
APP_BEGIN : origin = 0x088000, length = 0x000002
APP_BUFF : origin = 0x088002, length = 0x000020
FLASHE : origin = 0x088022, length = 0x00FFDD /* on-chip Flash */
//FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x010000 /* on-chip Flash */
//FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000121 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x004FFD
BOOT_FLAG : origin = 0x016FFD, length = 0x000002
//RAMGS7 : origin = 0x013000, length = 0x003FFD
// RAMGS8 : origin = 0x014000, length = 0x001000
// RAMGS9 : origin = 0x015000, length = 0x001000
// RAMGS10 : origin = 0x016000, length = 0x001000
// RAMGS11 : origin = 0x017000, length = 0x000FF8 /* Uncomment for F28374D, F28376D devices */
// RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
RAMGS11 : origin = 0x017000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
/* ALA_SRAM : origin = 0x100000, length = 0x040000 */ /* CS2:2M,外部RAM实际256k*16bit, 实际使用32k */
/* USER_XRAM : origin = 0x00300000, length = 0x10000 */ /* CS3:512k*16bit, 实际使用仅0x180 */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0, ALIGN(8)
.text : > FLASHA PAGE = 0, ALIGN(8)
codestart : > BEGIN PAGE = 0, ALIGN(8)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.switch : > FLASHA PAGE = 0, ALIGN(8)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
#if defined(__TI_EABI__)
.init_array : > FLASHD, PAGE = 0, ALIGN(8)
.bss : > RAMGS5, PAGE = 1
.bss:output : > RAMGS5, PAGE = 0
.bss:cio : > RAMGS5, PAGE = 1
.data : > RAMGS5, PAGE = 1
.sysmem : > RAMGS5, PAGE = 1
/* Initalized sections go in Flash */
.const : > FLASHD, PAGE = 0, ALIGN(8)
#else
.pinit : > FLASHA, PAGE = 0, ALIGN(8)
// .ebss : >> RAMLS5 | RAMGS0 | RAMGS1 , PAGE = 1
.ebss : > RAMGS6 , PAGE = 1
.esysmem : > RAMLS4, PAGE = 0
.cio : > RAMLS4, PAGE = 0
/* Initalized sections go in Flash */
.econst : >> FLASHA PAGE = 0, ALIGN(8)
#endif
Filter_RegsFile : > RAMGS6, PAGE = 1
SHARERAMGS0 : > RAMGS6, PAGE = 1
SHARERAMGS1 : > RAMGS6, PAGE = 1
SHARERAMGS2 : > RAMGS6, PAGE = 1
ramgs0 : > RAMGS6, PAGE = 1
ramgs1 : > RAMGS6, PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASHA,
RUN = RAMGS5,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#else
/**** .TI.ramfunc : {} LOAD = FLASHA,
RUN = RAMLS6,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
***/
GROUP
{
.TI.ramfunc
{ -l F021_API_F2837xD_FPU32.lib}
} LOAD = FLASHA,
RUN = RAMLS4,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif
#else
ramfuncs : LOAD = FLASHA,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(8)
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
#if 0
/* The following section definition are for SDFM examples */
Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
#endif
bootdata : > BOOT_FLAG, PAGE = 1
app_buff : > APP_BUFF, PAGE = 0
/* AlaDataRegsFile : > ALA_SRAM , PAGE = 1 */
/* UserRamRegsFile : > USER_XRAM , PAGE = 1 */
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
目前为您找到了这个文档,里面有提到dataonly和ECC。