我使用
Fapi_doMarginRead函数读取flash中含有“0”的数据时发现会出现这一个word中出现某个bit被异常置为1的情况
我是使用读取函数读取了100个字放到ram中,和memory browser窗口中监控到的数据做对比


我使用的代码是这样的

但是使用直接取地址的方式,一个字一个字的读取好像就没问题,希望能得到你们的帮助,非常感谢。
我已经上传了cmd文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用
MEMORY { PAGE 0 : /* Program Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */ /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x000123, length = 0x0002DD RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS0 : origin = 0x008000, length = 0x002000 /* RAMLS1 : origin = 0x008800, length = 0x000800*/ /* RAMLS2 : origin = 0x009000, length = 0x000800 */ /* RAMLS3 : origin = 0x009800, length = 0x000800 */ RAMLS4 : origin = 0x00A000, length = 0x001000 //RAMLS5 : origin = 0x00A800, length = 0x000800 RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ // RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ FLASHA : origin = 0x080002, length = 0x003FFE /* on-chip Flash */ //FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */ FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */ FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */ APP_BEGIN : origin = 0x088000, length = 0x000002 APP_BUFF : origin = 0x088002, length = 0x000020 FLASHE : origin = 0x088022, length = 0x00FFDD /* on-chip Flash */ //FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASHG : origin = 0x098000, length = 0x010000 /* on-chip Flash */ //FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */ FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */ FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */ FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */ // FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */ BOOT_RSVD : origin = 0x000002, length = 0x000121 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMD1 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x001000 RAMGS1 : origin = 0x00D000, length = 0x001000 RAMGS2 : origin = 0x00E000, length = 0x001000 RAMGS3 : origin = 0x00F000, length = 0x001000 RAMGS4 : origin = 0x010000, length = 0x001000 RAMGS5 : origin = 0x011000, length = 0x001000 RAMGS6 : origin = 0x012000, length = 0x004FFD BOOT_FLAG : origin = 0x016FFD, length = 0x000002 //RAMGS7 : origin = 0x013000, length = 0x003FFD // RAMGS8 : origin = 0x014000, length = 0x001000 // RAMGS9 : origin = 0x015000, length = 0x001000 // RAMGS10 : origin = 0x016000, length = 0x001000 // RAMGS11 : origin = 0x017000, length = 0x000FF8 /* Uncomment for F28374D, F28376D devices */ // RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMGS11 : origin = 0x017000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 /* ALA_SRAM : origin = 0x100000, length = 0x040000 */ /* CS2:2M,外部RAM实际256k*16bit, 实际使用32k */ /* USER_XRAM : origin = 0x00300000, length = 0x10000 */ /* CS3:512k*16bit, 实际使用仅0x180 */ } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHA PAGE = 0, ALIGN(8) .text : > FLASHA PAGE = 0, ALIGN(8) codestart : > BEGIN PAGE = 0, ALIGN(8) /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 .switch : > FLASHA PAGE = 0, ALIGN(8) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ #if defined(__TI_EABI__) .init_array : > FLASHD, PAGE = 0, ALIGN(8) .bss : > RAMGS5, PAGE = 1 .bss:output : > RAMGS5, PAGE = 0 .bss:cio : > RAMGS5, PAGE = 1 .data : > RAMGS5, PAGE = 1 .sysmem : > RAMGS5, PAGE = 1 /* Initalized sections go in Flash */ .const : > FLASHD, PAGE = 0, ALIGN(8) #else .pinit : > FLASHA, PAGE = 0, ALIGN(8) // .ebss : >> RAMLS5 | RAMGS0 | RAMGS1 , PAGE = 1 .ebss : > RAMGS6 , PAGE = 1 .esysmem : > RAMLS4, PAGE = 0 .cio : > RAMLS4, PAGE = 0 /* Initalized sections go in Flash */ .econst : >> FLASHA PAGE = 0, ALIGN(8) #endif Filter_RegsFile : > RAMGS6, PAGE = 1 SHARERAMGS0 : > RAMGS6, PAGE = 1 SHARERAMGS1 : > RAMGS6, PAGE = 1 SHARERAMGS2 : > RAMGS6, PAGE = 1 ramgs0 : > RAMGS6, PAGE = 1 ramgs1 : > RAMGS6, PAGE = 1 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 #if defined(__TI_EABI__) .TI.ramfunc : {} LOAD = FLASHA, RUN = RAMGS5, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(8) #else /**** .TI.ramfunc : {} LOAD = FLASHA, RUN = RAMLS6, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) ***/ GROUP { .TI.ramfunc { -l F021_API_F2837xD_FPU32.lib} } LOAD = FLASHA, RUN = RAMLS4, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) #endif #else ramfuncs : LOAD = FLASHA, RUN = RAMLS0, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) #endif #endif /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } #if 0 /* The following section definition are for SDFM examples */ Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111 Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222 Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333 Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444 Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333 #endif bootdata : > BOOT_FLAG, PAGE = 1 app_buff : > APP_BUFF, PAGE = 0 /* AlaDataRegsFile : > ALA_SRAM , PAGE = 1 */ /* UserRamRegsFile : > USER_XRAM , PAGE = 1 */ } /* //=========================================================================== // End of file. //=========================================================================== */
目前为您找到了这个文档,里面有提到dataonly和ECC。