This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Error exist when importing the official C2000 example routines

Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE

 I'm using CCS version 12.2.0. I've installed C2000Ware_DigitalPower_SDK_5_03_00_00 and can see its path in the products interface.  However, when I import the projectspec file from the official C2000 example routines, I get an error message saying "See details below... clb_ex1_combinatorial_logic Product C2000WARE v0.0 is not currently installed and no compatible version is available. Please install this product or a compatible version." What should I do?