This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: F280049C光伏逆变使用?

Part Number: TMS320F280049C


关于使用SiC器件高开关频率下处理器采样问题请教

 1、开关频率为20kHz时的采样方式:

由于逆变器反馈电流为环内电流,含有大量的高频分量,所以在AD采样时避免频率混叠造成的影响,必须反馈电流的工频值,而在三角载波的波峰或波谷处采样,则可以自然的采样到中间值。

如果不按定点反馈来执行,则必然引入高频扰动;和混叠引起的低频扰动;

    这样的就是一个开关周期采样一次,执行一次控制计算。这样的基础是开关频率低,时间够长,Tsw=50us,可以完成一次计算。

 

2、开关频率为50kHz时的采样方式

在高的开关频率下,比如fsw=50kHz,那么Tsw就只有20us了,无法完成计算。所以,这种控制方式大概率会是控制频率比实际的开关频率低,采样频率也低,这样就会引起频率混叠,对控制系统造成干扰,如何解决?

 3、对于多路MPPT的光伏逆变器的直流电流采样问题说明

光伏逆变器可能有多大10几路的MPPT,这种控制通常会对各路boost的载波进行相位交错,这样就会造成固定位置采样方法的困难。很难调整载波相位满足所有MPPT的固定位置采样,我们就必须将AD采样调理电路的RC参数调的很大,尽量把开关纹波滤除,就会造成控制延迟很大,相位裕度很差,如何解决?