TI的专家您好!
最近在TMS320F280049C中配置看门狗的超时复位后,但一直没有生效。
代码如下,麻烦帮忙看下是哪里出了问题?谢谢了!
void Watchdog_Init(void) { //请参考技术手册216页对看门狗的详细说明 //超时时间计算:256*64 / INTOSC1(10MHz) * 512 = 0.8388608秒 WdRegs.WDCR.bit.WDCHK = 0x5; WdRegs.WDCR.bit.WDPRECLKDIV = 15;//Watchdog Clock Pre-divider = 256 WdRegs.WDCR.bit.WDPS=7;//Watchdog Clock Prescaler = 64 // // Connect the watchdog to the WAKEINT interrupt of the PIE // Write to the whole SCSR register to avoid clearing WDOVERRIDE bit // EALLOW; WdRegs.SCSR.bit.WDOVERRIDE =1; WdRegs.SCSR.bit.WDENINT = 0;//to trigger a reset EDIS; // // Enable the watchdog // EALLOW; //WdRegs.WDCR.all = 0x0028; WdRegs.WDCR.bit.WDDIS = 0; EDIS; // // Enable WAKEINT in the PIE: Group 1 interrupt 8 // Enable INT1 which is connected to WAKEINT: // //PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block //PieCtrlRegs.PIEIER1.bit.INTx8 = 1; // Enable PIE Group 1 INT8 //IER |= M_INT1; // Enable CPU INT1 //EINT; // Enable Global Interrupts // // Reset the watchdog counter // ServiceDog(); }