如题所示,我是利用EMIF对SRAM进行写入,当我写入小于65536个数据就可以正常写入,超过65536个数据就不行,就会卡在图里面的for循环中,但是length的定义length_t是灰色的,又无法知道他是什么类型,我该怎么办呢?我怀疑就是length_t的长度不够,65536刚好就是16位,里面的CHAR_BIT怎么修改呢?
/*****************************************************************************/ /* copy_decompress_lzss.c */ /* */ /* Copyright (c) 2006 Texas Instruments Incorporated */ /* http://www.ti.com/ */ /* */ /* Redistribution and use in source and binary forms, with or without */ /* modification, are permitted provided that the following conditions */ /* are met: */ /* */ /* Redistributions of source code must retain the above copyright */ /* notice, this list of conditions and the following disclaimer. */ /* */ /* Redistributions in binary form must reproduce the above copyright */ /* notice, this list of conditions and the following disclaimer in */ /* the documentation and/or other materials provided with the */ /* distribution. */ /* */ /* Neither the name of Texas Instruments Incorporated nor the names */ /* of its contributors may be used to endorse or promote products */ /* derived from this software without specific prior written */ /* permission. */ /* */ /* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS */ /* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT */ /* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR */ /* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT */ /* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, */ /* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT */ /* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, */ /* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY */ /* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT */ /* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE */ /* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* */ /* */ /* Decompress routine for Lempel-Ziv-Storer-Szymanski (LZSS) compression. */ /* Given an input buffer with data compressed using LZSS encoding and an */ /* output buffer, this routine decompresses the data in the output buffer. */ /* */ /* NOTE: */ /* 1. This routine could be used to copy uninitialized or initialized global */ /* data space of a program. Hence this routine cannot define any global */ /* variable. */ /* 2. This routine will never be used to initialize stack space and hence */ /* all the variables are allocated to stack. */ /* 3. The calling application should ensure the output buffer is big */ /* enough to hold the uncompressed data. */ /* */ /*****************************************************************************/ #include <stdint.h> #include <limits.h> #define LZSS_EOD 4095 #define LZSS_WINDOW_SIZE 4095 /*****************************************************************************/ /* The offset is always 12-bits so use a 16-bit type. */ /*****************************************************************************/ typedef uint_fast16_t offset_t; #if CHAR_BIT == 8 /*****************************************************************************/ /* The max length is 2^15-1+18, which can fit in a 16-bit type. */ /*****************************************************************************/ typedef uint_fast16_t length_t; /*****************************************************************************/ /* Flags is always of length 1 char. */ /*****************************************************************************/ typedef uint_fast8_t flags_t; #elif CHAR_BIT == 16 /*****************************************************************************/ /* The max length =s 2^16-1+17, which may not fit in a 16-bit type, so use a */ /* 32-bit type. */ /*****************************************************************************/ typedef uint_fast32_t length_t; /*****************************************************************************/ /* Flags is always of length 1 char. */ /*****************************************************************************/ typedef uint_fast16_t flags_t; #else #error Illegal value for CHAR_BIT #endif /*****************************************************************************/ /* MSP copy tables can handle moving functions even in small data model + */ /* large code model, where data pointers are not big enough to represent */ /* function pointers. This requires the EABI decompression functions */ /* (SHARED/copy_*.c) to be changed to accept "far" pointers. For this */ /* memory model combination, the decompression functions are changed to use */ /* "unsigned long" to represent function pointers, so function pointers */ /* through which we call these functions also needs to have a prototype */ /* accepting "unsigned long" instead of pointer types. All other memory */ /* model combinations use the same prototype that all the other targets use: */ /* two data pointer arguments. Ultimately we use MSP peek/poke intrinsics */ /* to read/write the "far" memory. */ /*****************************************************************************/ #if defined(__MSP430__) && defined(__LARGE_CODE_MODEL__) && !defined(__LARGE_DATA_MODEL__) typedef unsigned long pointer_t; typedef unsigned long pointer_to_const_t; #define READ_CHAR_ADV(x) __data20_read_char(x++) #define WRITE_CHAR_ADV(x, c) __data20_write_char(x++, c) #else typedef unsigned char *pointer_t; typedef const unsigned char *pointer_to_const_t; #define READ_CHAR_ADV(x) (*x++) #define WRITE_CHAR_ADV(x,c) (*x++ = (c)) #endif /*****************************************************************************/ /* */ /* __TI_DECOMPRESS_LZSS() - Decompress data encoded using LZSS encoding. */ /* Input buffer (inbuf) has the encoded data and */ /* uncompressed data is returned in outbuf. */ /* */ /*****************************************************************************/ __attribute__((section(".text:decompress:lzss"))) void __TI_decompress_lzss(pointer_to_const_t inbuf, pointer_t outbuf) { while (1) { flags_t flags = READ_CHAR_ADV(inbuf); int i; for (i=0; i<CHAR_BIT ; i++) { if (flags & 0x1) { /*---------------------------------------------------------------*/ /* We have an uncoded byte, just write it out. */ /*---------------------------------------------------------------*/ WRITE_CHAR_ADV(outbuf, READ_CHAR_ADV(inbuf)); } else { /*---------------------------------------------------------------*/ /* Read and unpack the offset and length */ /*---------------------------------------------------------------*/ offset_t offset; length_t length; #if CHAR_BIT == 8 offset = READ_CHAR_ADV(inbuf); length = READ_CHAR_ADV(inbuf); offset <<= 4; offset |= ((length & 0x00F0) >> 4); length = (length & 0x000F) + 3; /*---------------------------------------------------------------*/ /* If the length is 3->17, we only use 4 bits. If the length is */ /* >= 18, we read an additional 8 bits and add it to the length. */ /* */ /* If the msb of the second byte is 1, we read an additional */ /* 8 bits and use that for bits 7-14 of the length. This gives */ /* us a range of 3->32785. */ /*---------------------------------------------------------------*/ if (length == 18) { length_t length2 = READ_CHAR_ADV(inbuf); if (length2 & 0x80) { length_t length3 = READ_CHAR_ADV(inbuf); length2 = (length2 & 0x7f) | (length3 << 7); } length += length2; } #elif CHAR_BIT == 16 unsigned char temp = READ_CHAR_ADV(inbuf); length = (temp & 0xf) + 2; offset = temp >> 4; /*---------------------------------------------------------------*/ /* If the length is the maximum value encoded in 4 bits, read an */ /* additional 16-bit value and add it to the length. */ /*---------------------------------------------------------------*/ if (length == 17) length += READ_CHAR_ADV(inbuf); #endif /*---------------------------------------------------------------*/ /* If the offset indicates end of data, exit. */ /*---------------------------------------------------------------*/ if (offset == LZSS_EOD) return; /*---------------------------------------------------------------*/ /* Copy the decoded string from sliding window to output buffer. */ /*---------------------------------------------------------------*/ length_t j; pointer_t pos = outbuf - offset - 1; for (j = 0; j < length; j++) WRITE_CHAR_ADV(outbuf, READ_CHAR_ADV(pos)); } flags >>= 1; } } }
请问copy_decompress_lzss.c这个文件是什么作用?以及是在main函数运行之前启用吗?为什么我会卡在这个文件里面呢?
您好,
长度为16位。 请参阅以下链接中的14.3 (压缩数据格式):
C28x Embedded Application Binary Interface (Rev. B)
copy_decompress_lzss.c 是 RTS 库的一部分、应进行修改。 否则、您必须重新构建 RTS 库。
你好,请问怎么修改为32位呢?但是我看了limits.h 定义的char_bit为16位,按照LZSS文件的定义typedef uint_fast32_t length_t;应该是32位,但是呢为什么LZSS文件是灰色呢?是否存在定义不成功
您好,
所有 CCS 项目都需要 RTS (运行时库)。 如果启用了 FPU (浮点)、则应选择 rts2800_fpu32_eabi.lib。
对于 TMS320C2000、char_bit 为16。