This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
“
epwm1_info.EPwm_CMPA_Direction = EPWM_CMP_UP; // Start by increasing CMPA &
epwm1_info.EPwm_CMPB_Direction = EPWM_CMP_DOWN; // decreasing CMPB
epwm1_info.EPwmTimerIntCount = 0; // Zero the interrupt counter
epwm1_info.EPwmRegHandle = &EPwm1Regs; // Set the pointer to the ePWM module
epwm1_info.EPwmMaxCMPA = EPWM1_MAX_CMPA; // Setup min/max CMPA/CMPB values wsf
epwm1_info.EPwmMinCMPA = EPWM1_MIN_CMPA;
epwm1_info.EPwmMaxCMPB = EPWM1_MAX_CMPB;
epwm1_info.EPwmMinCMPB = EPWM1_MIN_CMPB;
”
在epwm配置中,以上代码的作用是什么?
这用于了解计数器的方向(递增计数器或递减计数器用于递增计数模式),在示例的运行时更改时设置最小/最大计数器比较值。
MaxCMPA/B和Min CMPA/B用于控制PWM的占空比。