This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28384D: DAC没有输出

Part Number: TMS320F28384D


在CCS上下载例程【buffdac_ex1_enable】,在示波器上观测DAC的输出

修改DAC的值,示波器上的波形没有变化,请问是哪里不对?

DAC初始化的代码如下:

void myDAC0_init()

{
    //
    // Set DAC reference voltage.
    //
    DAC_setReferenceVoltage(myDAC0_BASE, DAC_REF_VDAC);
    //
    // Set DAC load mode.
    // 
    DAC_setLoadMode(myDAC0_BASE, DAC_LOAD_SYSCLK);
    //
    // Enable the DAC output
    //
    DAC_enableOutput(myDAC0_BASE);
    //
    // Set the DAC shadow output
    //
    DAC_setShadowValue(myDAC0_BASE, 0U);

    //
    // Delay for buffered DAC to power up.
    //
    DEVICE_DELAY_US(500);
}