异步电机参数学习中发现EST_Rs_State_Coarse与EST_Rs_State_Fine过程的实际电流幅值不对,不像下图中那样,而是USER_MOTOR_RES_EST_CURRENT设置值的一半,即按下图EST_Rs_State_Coarse与EST_Rs_State_Fine过程的实际电流幅值是0.5A,而不是1A。且发现EST_Rs_State_RampUp的时间值是不可调的,改成2后EST_Rs_State_RampUp的时间也是1秒。请诸位指教~谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
异步电机参数学习中发现EST_Rs_State_Coarse与EST_Rs_State_Fine过程的实际电流幅值不对,不像下图中那样,而是USER_MOTOR_RES_EST_CURRENT设置值的一半,即按下图EST_Rs_State_Coarse与EST_Rs_State_Fine过程的实际电流幅值是0.5A,而不是1A。且发现EST_Rs_State_RampUp的时间值是不可调的,改成2后EST_Rs_State_RampUp的时间也是1秒。请诸位指教~谢谢
我们在用的是motorware_1_01_00_14,这个应该是motorware 14吧,没有用motorware 15 .这两个是有重要的差别的么?
恩,我们在学习的时候是在lock rotor提示后把转子卡死后再置标志位继续学习的,而且也都是在空载的时候学习的。只是按照学习到的参数更新use.h后,空载时运行到目标转速时实际测到的与ccs反馈的转速还是一致的,只是随着加载量的增大实际测到的转速下降越来越大(1000转时加载10Nm下降到860转,而ccs反馈的Speed_krpm仍为1000转左右)。感觉加载时转速估算就不准确了,不知是否跟SpinTAC调速有关系,也在尝试改成lab5b FOC例程进行转速调节。