Part Number: LM3485
Hi Team.
Now add two questions
1, this model is suitable for solar photovoltaic products of this kind, the specifications did not see
2, in the material of the periphery added a 2.5 ohm series resistance (normal, not allowed), FB pin access to the MCU control signals (the original factory does not have this type of design reference), please ask whether this design is permitted, because do not add a series resistance simply test the material itself is not a problem! This is the latest update of this information!



![]()

这个是昨天你这边说要的那个图纸,标出来的地方是外围加的串联电阻,我把上在的截图改成英文的了,整理成一个表格,我怎么发你,我好像没找到途径