This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3485: Updated information

Part Number: LM3485

Hi Team.

Now add two questions
1, this model is suitable for solar photovoltaic products of this kind, the specifications did not see
2, in the material of the periphery added a 2.5 ohm series resistance (normal, not allowed), FB pin access to the MCU control signals (the original factory does not have this type of design reference), please ask whether this design is permitted, because do not add a series resistance simply test the material itself is not a problem! This is the latest update of this information!